Thought Leadership

Part 10: The 2016 Wilson Research Group Functional Verification Study

IC/ASIC Language and Library Adoption Trends

This blog is a continuation of a series of blogs related to the 2016 Wilson Research Group Functional Verification Study (click here).  In my previous blog, I focused on I various verification technology adoption trends. In this blog I plan to discuss various IC/ASIC language and library adoption trends.

Fig. 10-1 shows the adoption trends for languages used to create RTL designs. Essentially, the adoption rates for all languages used to create RTL designs is projected to be either declining or flat over the next year.

BLOG-2016-WRG-figure-10-1
Fig. 10-1. IC/ASIC Languages Used for RTL Design

As previously noted, the reason some of the results sum to more than 100 percent is that some projects are using multiple languages; thus, individual projects can have multiple answers.

Fig. 10-2 shows the adoption trends for languages used to create IC/ASIC testbenches. Essentially, the adoption rates for all languages used to create testbenches are either declining or flat. Furthermore, the data suggest that SystemVerilog adoption is starting to saturate or level off in the mid-70s range.

BLOG-2016-WRG-figure-10-2
Fig. 10-2. IC/ASIC Languages Used for Verification (Testbenches)

IC/ASIC Testbench Methodologies

Fig. 10-3 shows the adoption trends for various IC/ASIC testbench methodologies built using class libraries.

BLOG-2016-WRG-figure-10-3
Fig. 10-3. IC/ASIC Methodologies and Testbench Base-Class Libraries

Here we see a decline in adoption of all methodologies and class libraries with the exception of Accellera’s UVM, whose adoption continued to increase between 2014 and 2016. Furthermore, our study revealed that UVM is projected to continue its growth over the next year. However, like SystemVerilog, it will likely start to level off in the mid- to upper-70 percent range.

Assertion Languages

Fig. 10-4 shows the IC/ASIC industry adoption trends for various assertion languages, and again, SystemVerilog Assertions seems to have saturated or leveled off.

BLOG-2016-WRG-figure-10-4
Fig. 10-4. IC/ASIC Assertion Language Adoption

In my next blog, I plan to present the IC/ASIC design and verification power trends.

Quick links to the 2016 Wilson Research Group Study results

Harry Foster
Chief Scientist Verification

Harry Foster is Chief Scientist Verification for Siemens Digital Industries Software; and is the Co-Founder and Executive Editor for the Verification Academy. Harry served as the 2021 Design Automation Conference General Chair, and is currently serving as a Past Chair. Harry is the recipient of the Accellera Technical Excellence Award for his contributions to developing industry standards. In addition, Harry is the recipient of the 2022 ACM Distinguished Service Award, and the 2022 IEEE CEDA Outstanding Service Award.

More from this author

Comments

2 thoughts about “Part 10: The 2016 Wilson Research Group Functional Verification Study

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2016/10/31/part-10-the-2016-wilson-research-group-functional-verification-study/