In the rapidly evolving field of semiconductor testing, the ability to adapt and optimize test strategies is crucial for achieving…
Boundary scan is an integral part of electronic circuit design, be it system level, PCB level, chip level or physical…
In today’s semiconductor manufacturing, the pursuit of perfection leaves no room for error. Traditional testing methodologies often miss subtle yet…
Concurrent BISR (Built-In Self-Repair) chains refer to a methodology that enables the simultaneous processing of multiple BISR chains during power-up,…
The BISR controller is at the heart of the Tessent Platform repair solution. It facilitates access to the BISR chains…
A tap controller, or Test Access Port (TAP) controller, is a critical component in the design-for-test (DFT) methodology used in…
By Minjung Han (minjung.han@siemens.com), Calibre Support Application Engineer 3D-IC technology is gaining attention as an alternative to complement Moore’s Law,…
By 한민정 과장 (minjung.han@siemens.com), Calibre Support Application Engineer 3D-IC 기술은 무어의 법칙이 물리적 한계에 가까워지면서 이를 보완하는 대안으로 주목받고 있습니다….
ATPG’s goal is to create a set of patterns that achieves a given test coverage, where test coverage is the…