Touch Temperature – Part 2: Coefficient of Thermal Spreading

A coefficient of thermal spreading and the psychology of hot spots, explained with the help of Simcenter Flotherm applied to handheld electronics and smartphones

Using water cooling in electronics thermal management – a PC cooling example

Water Cooling? Sounds intriguing, but can liquid cooling be an effective method for thermal management of a PC system? Short…

Are heat pipes any good for my CPU?

When researching improved heat sink design to cool a CPU in a model I am developing, a common theme I…

Using Simcenter Motorsolve

6 Things YNTK About Simcenter MAGNET & Motorsolve 2020.1

Improvements in demagnetization predictions, simulation of bus bars and loss exports for thermal analysis.

May the (magnetic) Force be with you

One of the most interesting manifestations of magnetic phenomena is the motion that a magnetic field induces on some bodies and materials. This effect is used in several industrial applications, but are you able to compute it?

The times they are a changin’

Learn more about semiconductor thermal characterization and lifetime testing to understand the way to component level reliability.

Utilizing CFD to analyze a PC Cooling System

Investigating PC cooling system performance using computational fluid dynamics CFD simulation software to predict airflow and CPU temperature.

Creating a CPU thermal model from scratch quickly

CPU created in Simcenter Flotherm Package Creator The most important component within a typical PC computer is the CPU. So…

PC cooling: CPU cooler CFD simulation

Is my PC too hot?

Well, it depends on how you are using the PC. I’m Baptista De Noronha, and this is my new PC….