Pushing the Envelope: Maximizing efficiency with Finite Element Analysis (FEA)

There are a variety of definitions and interpretations of what efficiency means. In the simplest terms, it’s about being able…

Avoid Bearing failure with Virtual Prototyping. Angular Contact Ball Bearing (ACBB, left), Tapered Roll Bearing (TRB, right), as modeled in Simcenter 3D

Bearing Transmission Failures: How to Avoid Them With Virtual Prototyping

Bearings allow complex machinery to rotate by making the rotation possible while reducing friction, and are therefore vital to system efficiency and reliability. Improving bearing design through virtual prototyping is a cost-effective and thorough design approach, which reduces transmission downtime and failures.

Excellence in electric vehicle NVH at Karma Automotive

What should an electric sports car engine sound like? There is currently no clear answer to this question, as there is very little history of electric vehicles to draw from. Engine noise is also brand-specific, so even existing electric vehicles will sound different depending on which company produced them.

How Rule of Mixtures is Killing Your Composite Design

Rule of Mixtures is probably the most known and widespread method of estimating composite properties. Its notoriety in composite design circles is also its main problem: Rule of Mixtures has been overused and applied to cases that do not even come close to respecting its original, simplifying assumptions.

Fatigue Challenge of Additive Manufacturing

The Fatigue Challenge of Additive Manufacturing: A Simulation-Based Approach

Additive Manufacturing (AM), also known as 3D-printing, allows the production of complex components layer by layer, using only the material you need. Siemens Digital Industries Software offers simulation-based solutions to predict and optimize Additive Manufacturing product performance.

Multiscale Analysis: A General Overview and Its Applications in Material Design

Modeling advanced materials accurately is extremely complex. Multiscale simulations achieve balance between simulation accuracy and computational efficiency by capturing their behavior and important features at multiple scales.

High Velocity Impact on Composites – Past, Present, and Future

In 1969, Grumman Aerospace was the first company to successfully introduce advanced composites into a commercial airplane. The boron-epoxy laminated horizontal stabilizer used in the F-14A was 15% lighter and 18% less costly than its metal counterpart.

Accelerate Airworthiness Certification

Accelerating Airworthiness Certification

Changing the Game: Bye Aerospace wants to be the first FAA-certified electric aircraft by accelerating airworthiness certification using Simcenter.

Jet Engine Efficiency: Making Cleaner Skies the ‘New Normal’ Part II

Last week, I described how the current global pandemic provided one bright spot: the reduction in CO2 emissions. For such…