Fatigue Challenge of Additive Manufacturing

The Fatigue Challenge of Additive Manufacturing: A Simulation-Based Approach

Additive Manufacturing (AM), also known as 3D-printing, allows the production of complex components layer by layer, using only the material you need. Siemens Digital Industries Software offers simulation-based solutions to predict and optimize Additive Manufacturing product performance.

Rendering of the Chengdu ADAS MIL SIL test and demo lab

Chengdu: ADAS lab to test and validate performance

Get a glimpse of the ADAS demonstrator and test lab at the Chengdu AV/EV Engineering Center. This is article 2 of the Chengdu blog post series.

High Velocity Impact on Composites – Past, Present, and Future

In 1969, Grumman Aerospace was the first company to successfully introduce advanced composites into a commercial airplane. The boron-epoxy laminated horizontal stabilizer used in the F-14A was 15% lighter and 18% less costly than its metal counterpart.

ABEC engineers configure a custom bioreactor.

Beyond social distancing, simulations are already serving in the struggle

Learn how simulation has already played a crucial role in the the ongoing struggle against COVID-19.

High fidelity simulation using Simcenter Prescan C++ Simulation interface

With the release of Simcenter Prescan 2019.3, the C++ simulation interface was introduced, making it possible for users to run simulation without need for Matlab Simulink. This on demand webinar goes into this capability a little bit deeper and offers additional insight with use cases.

Accelerate Airworthiness Certification

Accelerating Airworthiness Certification

Changing the Game: Bye Aerospace wants to be the first FAA-certified electric aircraft by accelerating airworthiness certification using Simcenter.

Chengdu: building China’s Auto Silicon Valley

Construction of the automotive AV/EV Engineering Center in Chengdu has started. Check out here how Simcenter Engineering will deliver and operate several key application-oriented demonstrations and testing facilities to help build China’s Auto Silicon Valley.

rotor dynamics jet

The Beauty of Complexity

Gas turbine engines are beautiful. You’re probably thinking “that guy’s been stuck inside for too long,” but think about it…

Apollo 13 simulator

Apollo 13: The first digital twin

The behind the scenes story of how NASA used Digital Twin technology to bring a crippled spaceship safely home.