Assessing composite variability’s impact on performance with virtual testing

Statistics impact our world One of Albert Einstein’s most famous quotes is: “God does not play dice with the universe”….

Acoustic response of an ultrasonic parking sensor

Ray Acoustics Modeling: Exploring Performance in the Full Frequency Range

Ray Acoustics Modeling treats high frequency sound behavior as if it were a ray of light, which makes simulating acoustic performance in large environments feasible.

Avoid Bearing failure with Virtual Prototyping. Angular Contact Ball Bearing (ACBB, left), Tapered Roll Bearing (TRB, right), as modeled in Simcenter 3D

Bearing Transmission Failures: How to Avoid Them With Virtual Prototyping

Bearings allow complex machinery to rotate by making the rotation possible while reducing friction, and are therefore vital to system efficiency and reliability. Improving bearing design through virtual prototyping is a cost-effective and thorough design approach, which reduces transmission downtime and failures.

Digital Twins for Performance Engineering

Digital twins for performance engineering

Are you curious to learn more about the power of digital twins? Read about the upcoming Simcenter@RealizeLive.

Excellence in electric vehicle NVH at Karma Automotive

What should an electric sports car engine sound like? There is currently no clear answer to this question, as there is very little history of electric vehicles to draw from. Engine noise is also brand-specific, so even existing electric vehicles will sound different depending on which company produced them.

Chengdu: battery simulation lab revolutionizes battery design

How the Chengdu battery simulation demonstrator at the Chengdu engineering center can help electric vehicle automakers reduce development time considerably.

How Rule of Mixtures is Killing Your Composite Design

Rule of Mixtures is probably the most known and widespread method of estimating composite properties. Its notoriety in composite design circles is also its main problem: Rule of Mixtures has been overused and applied to cases that do not even come close to respecting its original, simplifying assumptions.

Fatigue Challenge of Additive Manufacturing

The Fatigue Challenge of Additive Manufacturing: A Simulation-Based Approach

Additive Manufacturing (AM), also known as 3D-printing, allows the production of complex components layer by layer, using only the material you need. Siemens Digital Industries Software offers simulation-based solutions to predict and optimize Additive Manufacturing product performance.

Multiscale Analysis: A General Overview and Its Applications in Material Design

Modeling advanced materials accurately is extremely complex. Multiscale simulations achieve balance between simulation accuracy and computational efficiency by capturing their behavior and important features at multiple scales.