Thought Leadership

Conclusion: The 2016 Wilson Research Group Functional Verification Study

Deeper Dive into First Silicon Success and Safety Critical Designs

This blog is a continuation of a series of blogs related to the 2016 Wilson Research Group Functional Verification Study (click here).  In my previous blog, I presented verification results in terms of schedules, number of required spins, and classification of functional bugs. In this blog, I conclude the series by having a little fun with some of the findings from our recent study.

You might recall from our 2014 study we did a deeper dive into the findings made a non-intuitive observation related to design size and first silicon success. That is, the smaller the design the less likelihood of achieving first silicon success (see 2014 conclusion blog for details). This observation still holds true in 2016.

For our 2016 study, we decided to do a deeper dive related to the following:

  1. Verification maturity and silicon success, and
  2. Safety critical designs and silicon successes.

Verification Maturity and Silicon Success

Fig. C-1 presents the findings for IC/ASIC first silicon success, and Fig. C-2 presents the findings for FPGA non-trivial bug escapes into production. It is important to note that only 33 percent of IC/ASIC projects are able to achieve first silicon success, and only 22 percent of FPGA projects go into production without a non-trivial bug.

BLOG-2016-WRG-figure-Con-1
Fig. C-1. IC/ASIC required spins before final production

BLOG-2016-WRG-figure-Con-2
Fig. C-2. FPGA non-trivial bug escapes into production

A question worth asking is if there might be some correlation between project success (in terms of preventing bugs) and verification maturity. To answer this question, we looked at verification technology adoption trends related to a project’s silicon success.

Fig. C-3 presents the adoption of various verification techniques related to IC/ASIC projects and then correlates these results against achieving first silicon success. The data suggest that the more mature an IC/ASIC project is in its adoption of verification technology the more likelihood of achieving first silicon success.

BLOG-2016-WRG-figure-Con-3
Fig. C-3. IC/ASIC spins and verification maturity

Similarly, in Fig. C-4 we examine the adoption of various verification techniques on FPGA projects, and then correlate these results against preventing non-trivial bug escapes into production. Again, the data suggest that the more mature an FPGA project is in its adoption of verification technology the more likelihood that a non-trivial bug will not escape into production.

BLOG-2016-WRG-figure-Con-4
Fig. C-4. FPGA non-trivial bug escapes into production and verification maturity

Safety Critical Designs and Silicon Success

The second aspect of our 2016 study that we decided to examine a little deeper relates to safety critical designs and their silicon success. Intuitively, one might think that the rigid and structured process required to adhere to one of the safety critical development processes (such as, DO-254 for Mil/Aero, ISO 26262 for automotive, IEC 60601 for medical, etc.) would yield higher quality in terms of preventing bugs and achieving silicon success.

Fig. C-5 shows the percentage of IC/ASIC and FPGA projects that claimed to be working on a safety critical design.

BLOG-2016-WRG-figure-Con-5
Fig. C-5. Percentage of projects working on safety critical designs

Keep in mind that the findings in Figure 5 do not represent volume in terms of silicon production—the data represents projects that claim to work under one of the safety critical development process standards.  Using this partition between projects working on non-safety critical and safety critical designs we decided to see how these two classes of projects compared in terms of preventing bugs.

Fig. C-6 compares the number of required spins for both safety critical and non-safety critical IC/ASIC designs. While Fig. C-7 compares the FPGA designs with non-trivial bug escapes for both safety critical and non-safety critical designs.

BLOG-2016-WRG-figure-Con-6
Fig. C-6. Requires IC/ASIC spins for safety critical vs. non-safety critical designs

 BLOG-2016-WRG-figure-Con-7
Fig. C-7. Non-trivial bug escapes for safety critical vs. non-safety critical FPGA designs

Clearly, the data suggest that a development process adopted to ensure safety does not necessarily ensure quality. Perhaps this is non-intuitive. However, to be fair, many of the safety critical features implemented in today’s designs are quite complex and increase the verification burden.

This concludes the findings from the 2016 Wilson Research Group Study.

Quick links to the 2016 Wilson Research Group Study results

Harry Foster
Chief Scientist Verification

Harry Foster is Chief Scientist Verification for Siemens Digital Industries Software; and is the Co-Founder and Executive Editor for the Verification Academy. Harry served as the 2021 Design Automation Conference General Chair, and is currently serving as a Past Chair. Harry is the recipient of the Accellera Technical Excellence Award for his contributions to developing industry standards. In addition, Harry is the recipient of the 2022 ACM Distinguished Service Award, and the 2022 IEEE CEDA Outstanding Service Award.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2017/01/03/conclusion-the-2016-wilson-research-group-functional-verification-study/