Thought Leadership

Verification IP: Why design teams buy instead of build

Verification IP is one of those categories that sounds simple until a project tries to live without it.

As interface standards become more complex, design teams face a familiar decision: build protocol and memory verification infrastructure internally or buy a reusable solution that is already aligned to the standard. For many teams, that decision affects schedule, engineering focus, and verification confidence just as much as it affects tooling.

When we say verification IP, we mean pre-built verification solutions for standards-based peripheral interconnect interfaces and memories. Instead of developing monitors, checkers, stimulus, coverage models, and protocol-specific test content from scratch, teams can use a ready-made solution to verify those interfaces more efficiently.

For teams working on PCI Express, Ethernet, CXL, UCIe, DDR, LPDDR, HBM, UALink, storage protocols, and chiplet-based systems, that matters more every year.

What is Verification IP?

Verification IP is a reusable verification solution for protocol and memory standards. It gives engineering teams pre-built components to verify standards-based interfaces faster than building those capabilities internally from scratch.

In practice, verification IP is used to verify how a design implements a standard interface or memory protocol. That may include stimulus generation, protocol checking, functional coverage, error handling, compliance-oriented testing, and debug support.

The biggest advantage is reuse. Instead of starting each new interface project with a blank page, teams can begin with verification content that is already focused on the protocol they need to validate.

That is especially important for standards that evolve quickly. A protocol is not just a signal list. It is a moving specification with detailed timing, behaviors, corner cases, and interoperability requirements. Verification IP helps teams keep up without turning every new standard into a custom internal development project.

Why do teams buy Verification IP instead of building it?

Teams buy verification IP because building and maintaining protocol verification infrastructure internally can consume major engineering time, especially when test suites grow into hundreds or thousands of cases.

Most experienced verification teams have done the build-vs-buy calculation. Building internally can look attractive at first, especially if the team wants maximum control. But the real cost is not only the first version. It is the maintenance burden that follows.

Standards change. New revisions appear. Integration environments shift from simulation into emulation. Compliance expectations rise. Debug demands get deeper. What began as an internal convenience can become a long-term ownership burden.

Verification IP lets teams buy a solution rather than build it from scratch for every standards-based interface.

For engineering leaders, the real question is usually not whether the team can build VIP. It is whether that is the best use of expert verification resources when schedules are tight and interface complexity keeps rising.

What should engineers look for in modern Verification IP?

Modern Verification IP should be evaluated on protocol coverage, spec currency, workflow reuse, emulation support, memory-model quality, ecosystem alignment, and vendor expertise.

A useful evaluation framework includes:

1. Breadth of standards coverage

A strong portfolio should cover the interfaces your roadmap actually depends on, not just legacy standards. This could include:

  • PCI Express
  • Ethernet
  • CXL
  • UCIe
  • Ultra Accelerator Link
  • Ultra Ethernet
  • DDR
  • LPDDR
  • HBM
  • flash variants
  • DIMM variants
  • UFS
  • eMMC
  • SD card
  • SDIO
  • NVMe-layered storage use cases

2. Spec readiness

For fast-moving standards, timing matters. Teams at the leading edge want verification solutions that track evolving specifications early, not months after the market has moved.

3. Reuse across verification platforms

If the same VIP can support both simulation and emulation, that improves continuity and protects testbench investment.

4. UVM-based methodology support

Avery Verification IP is SystemVerilog UVM-based. That matters because methodology alignment reduces friction for verification teams with established flows.

5. Memory ecosystem quality

For memory verification, current models and timing information matter. That is especially relevant when teams are validating controllers or SoC integration around third-party IP blocks.

6. Support for specialized and custom requirements

Not every team only uses mainstream protocols. Automotive, military, aerospace, and other high-reliability segments often need specialized support or custom development.

How does accelerated Verification IP extend the life of a testbench?

Accelerated verification IP helps teams reuse VIP, testbenches, and tests on emulation platforms so they can preserve prior work while gaining higher execution speed.

Avery Verification IP can run on the simulator and also on Siemens Veloce through an accelerated VIP approach. This matters because many teams invest heavily in creating a high-quality testbench, then face a second challenge when design size or software content makes simulation too slow.

If the verification environment can move to emulation without forcing a major rebuild, that extends the useful life of the original environment. The value is not just speed. It is continuity. Teams can carry forward VIP, reuse tests, and keep their debug context as the project scales.

Where does Verification IP matter most today?

Verification IP is especially important in fast-moving, standards-heavy markets such as AI/HPC, chiplets and 3D IC, memory subsystems, storage, automotive electronics, and specialized high-reliability systems.

1. AI and high-performance compute

    AI/HPC systems depend on high-bandwidth interconnect and memory technologies. That increases verification demand around PCI Express, CXL, UCIe, HBM, Ethernet, and newer scale-up and scale-out interconnects.

    2. Chiplets and 3D IC

    As 3D IC and chiplet-based design become more accessible, interface verification becomes a first-pass success issue. Teams need confidence in chiplet-to-chiplet communication, not just confidence in isolated blocks.

    3. Memory verification

    Memory interfaces remain foundational. Verification needs span controllers, PHY integration, SoC-level integration, and support for standards such as DDR, LPDDR, HBM, flash, and DIMM variants.

    4. Storage protocols

    Off-chip storage bandwidth keeps increasing, and the protocol stack is getting richer. Verification needs now span native storage interfaces and layered solutions such as NVMe on top of PCI Express.

    5. Automotive and specialized protocols

    Automotive programs often involve both established protocols and newer Ethernet-based standards. High-reliability sectors may also require custom or specialized protocol support.

    How does Verification IP support chiplet and 3D IC verification?

    In chiplet and 3D IC flows, verification IP helps teams validate die-to-die and system interfaces earlier so integration risk is reduced before silicon and package decisions are locked in.

    Chiplet-based systems create more interface boundaries. That means more opportunities for integration issues, interoperability gaps, and late-cycle debug. If you are creating chiplets, integrating SoCs or SiPs, or supporting 3D IC services, interface verification becomes central to first-pass success.

    What role can AI play around Verification IP?

    AI can improve how teams use verification IP by helping with debug, regression orchestration, and root-cause analysis, but it does not replace the need for robust VIP or experienced engineers.

    AI does not replace verification IP, and it does not replace the people using it. Instead, AI can improve productivity around the verification flow. That includes areas such as:

    • Regression efficiency
    • Coverage analysis support
    • Debug assistance
    • Property creation support
    • Protocol root-cause analysis

    Why Verification IP is still a strategic investment

    Verification IP remains strategic because interface complexity is rising faster than most teams can justify building and maintaining internal VIP for every protocol generation.

    Verification is not getting simpler. Standards keep moving. System integration keeps broadening. Interfaces increasingly sit at the center of AI, chiplet, memory, storage, and automotive design challenges.

    That means the value of verification IP is not only time savings at project start. It is long-term engineering leverage.

    For teams evaluating build versus buy, the better question is often this: where should scarce verification expertise create the most value? Writing and maintaining every protocol verification component internally may feel flexible, but it can also absorb years of effort that could be spent on differentiated design and system-level validation.

    Verification IP helps shift that balance.

    Conclusion

    Verification IP gives design teams a practical way to verify standards-based interfaces and memories without rebuilding the same infrastructure generation after generation.

    For organizations working across protocol-heavy SoC, chiplet, storage, memory, and AI/HPC designs, the value is clear: faster readiness, more reusable verification environments, better alignment to evolving standards, and less internal effort spent reinventing verification components that already need deep domain expertise.

    If your team is evaluating verification IP, focus on more than protocol names. Look at standards coverage, spec cadence, methodology fit, emulation reuse, memory-model quality, and the vendor’s ability to support both mainstream and emerging interfaces.

    That is where verification IP stops being a checkbox and becomes a real verification strategy decision.

    Key takeaways

    • Verification IP helps teams verify standards-based interfaces and memories without building everything internally.
    • The build-vs-buy decision is often about engineering time, spec complexity, and long-term maintenance.
    • Modern verification IP should support both protocol breadth and workflow reuse across simulation and emulation.
    • Chiplet, 3D IC, AI/HPC, storage, and automotive designs are increasing demand for robust interface verification.
    • AI is not a replacement for verification IP, but it can improve debug, regression efficiency, and root-cause analysis around the verification flow.

    Gordon Allan

    Gordon Allan is Director of Verification IP Product Management at Siemens EDA. Gordon was one of the original developers of Accellera UVM, and was responsible for Mentor's UVM Cookbook published on Verification Academy site and appreciated by over 40,000 engineers worldwide. Prior to joining the EDA industry in 2010 he gained over 18 years of SoC Design and Verification experience in lead engineer and senior consultant roles, working with many of the top semiconductor companies, fabless startups, system houses and EDA companies worldwide and giving him firsthand experience of customers’ challenges from spec to tapeout. Gordon is based in Silicon Valley.

    This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2026/05/18/verification-ip-why-design-teams-buy-instead-of-build/