Fatigue Challenge of Additive Manufacturing

The Fatigue Challenge of Additive Manufacturing: A Simulation-Based Approach

Additive Manufacturing (AM), also known as 3D-printing, allows the production of complex components layer by layer, using only the material you need. Siemens Digital Industries Software offers simulation-based solutions to predict and optimize Additive Manufacturing product performance.

Multiscale Analysis: A General Overview and Its Applications in Material Design

Modeling advanced materials accurately is extremely complex. Multiscale simulations achieve balance between simulation accuracy and computational efficiency by capturing their behavior and important features at multiple scales.

High Velocity Impact on Composites – Past, Present, and Future

In 1969, Grumman Aerospace was the first company to successfully introduce advanced composites into a commercial airplane. The boron-epoxy laminated horizontal stabilizer used in the F-14A was 15% lighter and 18% less costly than its metal counterpart.

Accelerate Airworthiness Certification

Accelerating Airworthiness Certification

Changing the Game: Bye Aerospace wants to be the first FAA-certified electric aircraft by accelerating airworthiness certification using Simcenter.

rotor dynamics jet

The Beauty of Complexity

Gas turbine engines are beautiful. You’re probably thinking “that guy’s been stuck inside for too long,” but think about it…

Jet Engine Efficiency: Making Cleaner Skies the ‘New Normal’ Part II

Last week, I described how the current global pandemic provided one bright spot: the reduction in CO2 emissions. For such…

Jet Engine Performance

Jet Engine Performance: Making Cleaner Skies the ‘New Normal’

One of the inadvertent effects of the current pandemic has been a drastic reduction in global air pollution. Amidst this…

Aero-engine sub-component design with the Mechanical Digital Twin

Challenges in Aero-engine engineering Aero-engines are complex machinery, largely because they experience deformations, include moving parts, and are subject to…

Simcenter 3D model of A 150 MVA Transformer

Simcenter 3D 2020.1 – Explore What’s New in Low Frequency Electromagnetics

New electric field analysis, improved electromagnetic-thermal coupling and EM-NVH