Multiscale Analysis: A General Overview and Its Applications in Material Design

Modeling advanced materials accurately is extremely complex. Multiscale simulations achieve balance between simulation accuracy and computational efficiency by capturing their behavior and important features at multiple scales.

Simcenter STAR-CCM+: 4 Keys to Handling Complex Geometry in your CFD Simulation

“Simplicity is the ultimate sophistication” – Leonardo da Vinci What does this mean for people tackling the ever-growing system complexity required to meet…

Rendering of the Chengdu ADAS MIL SIL test and demo lab

Chengdu: ADAS lab to test and validate performance

Get a glimpse of the ADAS demonstrator and test lab at the Chengdu AV/EV Engineering Center. This is article 2 of the Chengdu blog post series.

Are heat pipes any good for my CPU?

When researching improved heat sink design to cool a CPU in a model I am developing, a common theme I…

High Velocity Impact on Composites – Past, Present, and Future

In 1969, Grumman Aerospace was the first company to successfully introduce advanced composites into a commercial airplane. The boron-epoxy laminated horizontal stabilizer used in the F-14A was 15% lighter and 18% less costly than its metal counterpart.

system simulation for heavy equipment product development improvement

From heavy equipment component design to system integration with Simcenter Amesim

[Infographic] Discover how strong the footprint of system simulation is in the heavy equipment industry

High fidelity simulation using Simcenter Prescan C++ Simulation interface

With the release of Simcenter Prescan 2019.3, the C++ simulation interface was introduced, making it possible for users to run simulation without need for Matlab Simulink. This on demand webinar goes into this capability a little bit deeper and offers additional insight with use cases.

Chengdu: building China’s Auto Silicon Valley

Construction of the automotive AV/EV Engineering Center in Chengdu has started. Check out here how Simcenter Engineering will deliver and operate several key application-oriented demonstrations and testing facilities to help build China’s Auto Silicon Valley.

Automatic (CFD) for the People

Aerodynamic Database Generation for Aerospace Applications  It was mesmerizing.  Through the wind tunnel test section viewport, you could see the…