Excellence in electric vehicle NVH at Karma Automotive

What should an electric sports car engine sound like? There is currently no clear answer to this question, as there is very little history of electric vehicles to draw from. Engine noise is also brand-specific, so even existing electric vehicles will sound different depending on which company produced them.

How Rule of Mixtures is Killing Your Composite Design

Rule of Mixtures is probably the most known and widespread method of estimating composite properties. Its notoriety in composite design circles is also its main problem: Rule of Mixtures has been overused and applied to cases that do not even come close to respecting its original, simplifying assumptions.

Multiscale Analysis: A General Overview and Its Applications in Material Design

Modeling advanced materials accurately is extremely complex. Multiscale simulations achieve balance between simulation accuracy and computational efficiency by capturing their behavior and important features at multiple scales.

An insulated-gate bipolar transistor thermal simulation with Simcenter FLOEFD 2020.1, ready for a BCI-ROM extraction.

Simcenter™ FLOEFD™ 2020.1: What’s New?

The latest release of Simcenter FLOEFD 2020.1 has just been announced. Simcenter FLOEFD is a CAD-embedded computational fluid dynamics (CFD)…

High Velocity Impact on Composites – Past, Present, and Future

In 1969, Grumman Aerospace was the first company to successfully introduce advanced composites into a commercial airplane. The boron-epoxy laminated horizontal stabilizer used in the F-14A was 15% lighter and 18% less costly than its metal counterpart.

Accelerate Airworthiness Certification

Accelerating Airworthiness Certification

Changing the Game: Bye Aerospace wants to be the first FAA-certified electric aircraft by accelerating airworthiness certification using Simcenter.

Automatic (CFD) for the People

Aerodynamic Database Generation for Aerospace Applications  It was mesmerizing.  Through the wind tunnel test section viewport, you could see the…

Jet Engine Efficiency: Making Cleaner Skies the ‘New Normal’ Part II

Last week, I described how the current global pandemic provided one bright spot: the reduction in CO2 emissions. For such…

From design exploration to design thinking in 100s of CFD simulations

As we continue to evolve our “digital twin” assets, it might be helpful to ask, “How are we building our…