Thought Leadership

Part 7: The 2016 Wilson Research Group Functional Verification Study

IC/ASIC Design Trends

This blog is a continuation of a series of blogs related to the 2016 Wilson Research Group Functional Verification Study (click here). In my previous blog, I focused on FPGA design and verification trends.  I now will shift the focus of this series of blogs from FPGA trends to IC/ASIC trends.

In this blog, I present trends related to various aspects of design to illustrate growing design complexity. Fig. 7-1 shows the trends from the 2014 and 2016 studies in terms of active IC/ASIC design project by design sizes (gates of logic and datapath, excluding memories). Keep in mind that Fig. 7-1 represents design projects, not silicon volume.

IC/ASIC Design Size

One interesting observation from this year’s study is that there appeared to be a large increase in design projects working on designs less than 100K gates. This was somewhat of a surprise. Perhaps it is due to a number of projects working on smaller sensor chips for IoT devices. At any rate, it is important to keep this in mind when observing some of the verification technology adoption trends. The reason is typically these very small projects do not apply advanced verification techniques, which can bias the overall industry verification technique adoption trends in some cases.

BLOG-2016-WRG-figure-7-1
Fig. 7-1. IC/ASIC Design Sizes

The key takeaway from Fig. 7-1 is that the electronic industry continues to move to larger designs. In fact, 31 percent of today’s design projects are working on designs over 80M gates, while 20 percent of today’s design projects are working on designs over 500M gates.

But increased design size is only one dimension of the growing complexity challenge. What has changed significantly in design since the original Collett studies is the dramatic movement to SoC class of designs. In 2004, Collett found that 52 percent of design projects were working on designs that include one or more embedded processors. Our 2012 study found that the number of design projects working on designs with embedded processors had increased to 71 percent, and has been fairly consistent since that point in time as shown in Fig. 7-2.

IC/ASIC Embedded Processors

Another interesting trend is the increase in the number of embedded processes in a single SoC. For example, 49 percent of design projects today are working on designs that contain two or more embedded processors, while 16 percent of today’s designs include eight or more embedded processors. SoC class designs add a new layer of verification complexity to the verification process that did not exist with traditional non-SoC class designs due to hardware and software interactions, new coherency architectures, and the emergence of complex network on-a-chip interconnect.

BLOG-2016-WRG-figure-7-2
Fig. 7-2. IC/ASIC Design Sizes

IC/ASIC Asynchronous Clock-Domains

In addition to the increasing number of embedded processors contained within an SoC, it is not uncommon to find in the order of 120 integrated IP blocks within today’s more advanced SoCs. Many of these IP blocks have their own clocking requirements, which often present new verification challenges due to metastability issues involving signals that cross between multiple asynchronous clock-domains.

In Fig. 7-3, we see that 91 percent of all IC/ASIC design projects today are working on designs that have two or more asynchronous clock-domains.

BLOG-2016-WRG-figure-7-3
Fig. 7-3. Number of Asynchronous Clock-Domains in IC/ASIC Designs

One of the challenges with verifying clock-domain crossing issues is that there is a class of metastability bugs that cannot be demonstrated in simulation on an RTL model. To simulate these issues requires a gate-level model with timing, which is often not available until later stages in the design flow. However, static clock-domain crossing (CDC) verification tools have emerged as a solution used to automatically identify clock domain issues directly on an RTL model at earlier stages in the design flow.

In my next blog, I plan to discuss the growing IC/ASIC design project resource trends due to rising design complexity.

Quick links to the 2016 Wilson Research Group Study results

Harry Foster
Chief Scientist Verification

Harry Foster is Chief Scientist Verification for Siemens Digital Industries Software; and is the Co-Founder and Executive Editor for the Verification Academy. Harry served as the 2021 Design Automation Conference General Chair, and is currently serving as a Past Chair. Harry is the recipient of the Accellera Technical Excellence Award for his contributions to developing industry standards. In addition, Harry is the recipient of the 2022 ACM Distinguished Service Award, and the 2022 IEEE CEDA Outstanding Service Award.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2016/09/25/part-7-the-2016-wilson-research-group-functional-verification-study/