Thought Leadership

Part 12: The 2022 Wilson Research Group Functional Verification Study

IC/ASIC Verification Results Trends

This blog is a continuation of a series of blogs related to the 2022 Wilson Research Group Functional Verification Study (click here). In my previous blog, I provided data related to designs that actively manage power. In this blog, I present verification results findings in terms of schedules, number of required spins, and classification of functional bugs.

A metric often track to measure efficiency is IC/ASIC project completion compared to the original schedule, as shown in Fig. 12-1. Here we found that 66 percent of IC/ASIC projects were behind schedule, while 27% of projects were behind schedule by 27 percent.

Fig. 12-1. Design Completion Compared to Original Schedule

An additional metric often tracked to measure effectiveness is number of spins before production. Historically, for the past 20 years, about 30% of all IC/ASIC projects were able to achieve first silicon success. However, for 2022, only about 24 percent of today’s projects can achieve first silicon success. This is the lowest required spins percentage value recorded in the past twenty years! This, combined with the increasing wafer and mask cost, has become a huge concern.

IC/ASIC Respins

Fig. 12-2. Required Number of Spins

Fig. 12-3 shows various categories of design flaws contributing to IC/ASIC respins, where the percentage of “logic or functional flaws” remains the leading cause of bugs. In 2020 we began tracking flaws associated with safety and security features, and the data suggest a downward trend in term of these flaws in the 2022 study. Also, for the first time, we pulled out separately yield and reliability, so we cannot show trends at this time. Finally, obviously multiple flaws can contribute to bug escapes, which is the reason the total percentage of flaws sums to more than 100 percent.

Fig. 12-3. Types of Flaws Resulting in Respins

IC/ASIC Functional Flaws

Note that in 2020 we saw a huge increase in flaws attributed to tuning analog circuits. We were curious if this was an anomaly in the 2020 study. However, the issue repeated itself in our 2022 study. I analyzed this year’s results to see whether the spike was restricted to designs at the latest technology nodes, or if it was more widespread. It turns out that while 7nm or below was the most popular answer for those experiencing the problem, it only accounted for about 16% of the cases. Almost all nodes, including 150nm and larger, were seeing these types of failures. One possibility for this is the increasing amount of analog added to IC/ASIC regardless of node size.

The next thing I looked into was whether these issues existed in only smaller designs or larger ones. The results can be seen in Fig. 12-4 below. Nearly 50% of designs less than 1M gates experienced respins due to analog issues. This should not be too big of a surprise since automotive and IoT are driving a large demand for smaller sensor chips that include analog. However, a significant amount of designs larger than 1M gates are also experiencing response due to analog issues!

Fig. 12-4. Analog Flaws by Design Size

Fig. 12-5 demonstrates the root cause of logical or functional flaws by various categories. The data suggest design errors are the leading cause of functional flaws, and the situation is worsening. In addition, problems associated with changing, incorrect, and incomplete specifications are a common theme often voiced by many verification engineers and project managers.

Fig. 12-5. Root Cause of Functional Flaws

In my next blog, I provide some concluding remarks and observations.

Quick links to the 2022 Wilson Research Group Study results

Harry Foster
Chief Scientist Verification

Harry Foster is Chief Scientist Verification for Siemens Digital Industries Software; and is the Co-Founder and Executive Editor for the Verification Academy. Harry served as the 2021 Design Automation Conference General Chair, and is currently serving as a Past Chair. Harry is the recipient of the Accellera Technical Excellence Award for his contributions to developing industry standards. In addition, Harry is the recipient of the 2022 ACM Distinguished Service Award, and the 2022 IEEE CEDA Outstanding Service Award.

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2023/01/09/part-12-the-2022-wilson-research-group-functional-verification-study/