Thought Leadership

Part 9: The 2018 Wilson Research Group Functional Verification Study

IC/ASIC Verification Technology Adoption Trends

This blog is a continuation of a series of blogs related to the 2018 Wilson Research Group Functional Verification Study (click here).  In my previous blog, I focused on IC/ASIC design project resource trends. In this blog I examine IC/ASIC project verification technology adoption trends.

Dynamic Verification Techniques

The IC/ASIC market in the mid-2000 timeframe underwent growing pains to address increased verification complexity, predominately brought on with the adoption of SoC-class designs. This maturing of IC/ASIC projects’ processes is clearly visible when comparing various simulation-based verification technology adoption trends from 2007, 2012, and 2018, as shown in Fig. 9-1.


Fig. 9-1. IC/ASIC Verification Technology Adoption Trends (2007-2018)

Today we find that, in general, most IC/ASIC projects have matured and adopted a common set of simulation-based verification techniques as part of their IP and subsystem verification process. As the IC/ASIC industry matures, as expected, we see a trend of verification technology adoption peaking (that is, leveling off), as shown if Fig. 9-2.


Fig. 9-2. IC/ASIC Verification Technology Adoption Trends

As I mentioned in Part 7, for the past few studies we have seen a trend in terms of increased number of IC/ASIC projects working on designs less than 500K gates. It is important to keep in mind that these small projects often do not adopt advanced verification techniques, which can bias the overall industry verification technique adoption trends and appear as slight decline in adoption in some cases. The reality is that there has been little change in terms of adoption as the market matures.

IC/ASIC Static Verification Techniques

Fig. 9-3 shows the IC/ASIC adoption trends for formal property checking (e.g., model checking), as well as automatic formal applications. Examples of automatic formal application tools include: SoC integration connectivity checking, deadlock detection, X semantic safety checks, coverage reachability analysis, and many other properties that can be automatically extracted and then formally proven. Note, not included in the automatic formal application trend data are clock-domain crossing CDC tools.


Fig. 9-3. IC/ASIC Formal Technology Adoption

We see in Fig. 9-3 that formal property checking has grown at a 5.4 percent CAGR since 2012, while automatic formal applications has grown at a 9.2% CAGR. Again, keep in mind the previous discussion on increasing number of small projects, which are often less mature in their verification processes. As a result this can bias the adoption trends.

Emulation and FPGA Prototyping

According to Pedestal Research the Emulation market value was forecasted to be $376M in 2018, and expected to grow at a 7.6 percent CAGR over the next few years. Pedestal Research also claims that the FPGA Prototyping market value was forecasted to be $66M in 2018 (not including home grown solutions), and expected to grow at a 9.9 percent CAGR.

Historically, the simulation market has depended on processor frequency scaling as one means of continual improvement in simulation performance. However, as processor frequency scaling levels off, simulation-based techniques are unable to keep up with today’s growing complexity. This is particularly true when simulating large designs that include both software and embedded processor core models. Hence, acceleration techniques are now required to extend SoC verification performance for very large designs. In fact, emulation and FPGA prototyping have become key platforms for SoC integration verification where both hardware and software are integrated into a system for the first time. In addition to SoC verification, emulation and FPGA prototyping are also used today as a platform for software development.

Fig. 9-4 describes various reasons why projects are using emulation, while Figure 9-5 describes why FPGA Prototyping was performed. You might note that the results do not sum to 100 percent since multiple answers were accepted from each study participant.


Fig. 9-4. Why Was Emulation Performed?


Fig. 9-5. Why Was FPGA Prototyping Performed?

In my next blog, I plan to discuss various IC/ASIC language and library adoption trends.

Quick links to the 2018 Wilson Research Group Study results

Harry Foster
Chief Scientist Verification

Harry Foster is Chief Scientist Verification for Siemens Digital Industries Software; and is the Co-Founder and Executive Editor for the Verification Academy. Harry served as the 2021 Design Automation Conference General Chair, and is currently serving as a Past Chair. Harry is the recipient of the Accellera Technical Excellence Award for his contributions to developing industry standards. In addition, Harry is the recipient of the 2022 ACM Distinguished Service Award, and the 2022 IEEE CEDA Outstanding Service Award.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2019/02/05/part-9-the-2018-wilson-research-group-functional-verification-study/