Sequential optimisation is an alternative optimisation strategy that can be run in FloTHERM’s Command Center module. As with response surface…
To recap… So far in this series we’ve: Taken a simple FloTHERM application of a component+heatsink placed on a PCB…
A design of experiments based study will provide a scatter gun type indication of how the system performs with a…
Happy Chinese new year, wishing you all prosperity, luck, health and fortune in this, the year of the Monkey! Also…
The most effective, but least efficient, method to determine an optimal combination of design parameters is to consider every single…
Heatsinks are a very common method of aiding the transfer of heat from a source (e.g. IC die) to a…
There has been much talk about the appification of established technologies. Discussion on the appification of high-value CAE simulation seems…
A reliable electronic product is generally a cool one. In addition, one of the main limiters of non-functional performance is…
Available in the recently released FloTHERM V11.1 is the ability to calibrate a FloTHERM simulation model so that it matches…