Streamlining data: Efficient test data consolidation with Simcenter Testlab
As test engineers, whether working at the proving ground or on public roads, we gather a wealth of data. A complete measurement often includes various road conditions and numerous driving maneuvers. While acquiring this test data is a crucial first step, the real challenge often comes afterward: data consolidation. Traditionally, this means splitting long, continuous recordings into meaningful segments for analysis.

The challenges of manual test data consolidation
The process of consolidating test data can be surprisingly complex when done manually. After a day of intensive data acquisition, engineers face several hurdles:
- Manual data segmentation: Sifting through hours of recorded data to identify the precise start and end points of specific road conditions or maneuvers is a tedious and time-consuming task. This manual effort is prone to inconsistencies and can introduce errors, impacting the reliability of subsequent test data analysis.
- Inconsistent run naming: Once a segment is identified, giving it a clear, descriptive, and consistent name is another significant challenge. Without an automated system, engineers often resort to ad-hoc naming conventions, leading to confusion and making it difficult to locate and compare specific test runs later. This lack of structured naming can severely hinder efficient test data processing.
- Lack of automation: The biggest bottleneck in this traditional workflow is the absence of automation. Manual data consolidation not only consumes valuable engineering time but also diverts focus from higher-value analytical tasks.
These manual steps can delay your analysis, complicate collaboration, and ultimately slow down your development process. But what if there was a more efficient way to handle your test data consolidation?
Simcenter Testlab: Your solution for automated test data consolidation
This is where Simcenter Testlab offers a powerful and automated solution to transform your test data processing workflow. It turns those manual, time-consuming tasks into streamlined, efficient operations.
1. Automated data segmentation with GPS precision and Google Earth integration:
One of the standout features of Simcenter Testlab is its ability to automatically segment long measurement runs into meaningful portions using GPS coordinates. Your measured analog and digital data often includes precise GPS information. Simcenter Testlab intelligently uses this data to identify and cut your recordings based on predefined track sections or geographical areas.
The best part? Defining these precise geographical boundaries is incredibly straightforward. You can first identify the beginning and end of each track or specific road segment directly on Google Earth. Once you’ve marked these points, you simply save them as .kml and/or .kmz files. Then, you can easily open these files within Simcenter Testlab. With this information, Simcenter Testlab automatically cuts your measurements into portions that correspond exactly to the geographical segments you defined.

No more manual searching or guessing! This powerful integration ensures consistency and accuracy across all your data, especially valuable for both proving ground testing and public road testing. This capability truly streamlines automated data cutting and provides exact GPS coordinates for each separated run.
2. Intelligent naming for clear organization:
Beyond just cutting, Simcenter Testlab addresses the challenge of run naming head-on. It allows you to define intelligent naming conventions that are automatically applied to your segmented runs. Imagine your runs being automatically named like this:
ProvingGround_HighSpeedLoop_Run01PublicRoad_CityDriving_BumpySection_Run02Highway_OvertakeManeuver_Run03
This level of automatically generated detail makes finding and comparing specific test scenarios incredibly easy. You save significant time that would otherwise be spent on manual renaming and eliminate the ambiguity often found in manually organized files, greatly enhancing your overall test data consolidation.
3. Dynamic suffixes for driving maneuvers:
Simcenter Testlab further enhances data consolidation by allowing you to incorporate extra run suffixes based on driving maneuvers. This is incredibly useful for adding context to your data.
For instance, during a single run on a specific road segment, you might perform several different maneuvers: a hard brake, an acceleration, or a lane change. Simcenter Testlab can be configured to detect these maneuvers (often based on specific sensor data or pre-defined triggers) and automatically add a descriptive suffix to the run name. This could result in names such as:
ProvingGround_BrakingTest_EmergencyBrakePublicRoad_AccelerationTest_FullThrottleHighway_LaneChange_HighSpeed
This automated detail provides immediate context to your data, making post-processing and test data analysis significantly more efficient and insightful for test engineers.

See it in action: Automated data consolidation with Simcenter Testlab
Reading about these features is one thing, but seeing them in action truly highlights their power! To give you a clear understanding of how seamless and efficient this process can be, I’ve prepared a short video demonstration.
In this video, you’ll see:
- How to easily define track segments using Google Earth and import .kml/.kmz files into Simcenter Testlab.
- The automated process of splitting a long measurement into individual runs based on these precise GPS coordinates.
- How intelligent naming conventions are applied automatically.
- The magic of adding dynamic suffixes based on detected driving maneuvers.

The future of test data consolidation is automated
As you’ve seen, by leveraging the automation capabilities of Simcenter Testlab, test engineers can:
- Save Time: Drastically reduce the hours spent on manual data segmentation and naming.
- Improve accuracy: Minimize human error in data splitting and organization.
- Enhance consistency: Ensure uniform data structuring across all projects and teams.
- Accelerate analysis: Quickly locate and analyze specific test conditions and driving maneuvers.
- Boost productivity: Free up valuable engineering time to focus on understanding the data and making informed decisions.
If you’re looking to optimize your test data consolidation process, it’s time to explore how Simcenter Testlab can revolutionize your workflow. Say goodbye to manual struggles and hello to intelligent, automated test data processing!