Maximizing efficiency: accelerate your simulations with Simcenter Amesim 2410

Simcenter Amesim 2410 marks a significant leap forward in simulation efficiency and computational performance, with improvements tailored to address the ever-growing complexity of engineering systems. Here’s an overview of the key computational performance enhancements in this latest release.
Platform simulation acceleration
One of the major improvements in Simcenter Amesim 2410 comes from the platform-level simulation acceleration. This release introduces a new solver algorithm that significantly reduces redundant calculations. By reusing previously computed equational matrices, the software minimizes the need for repeated calculations, enhancing the overall speed of simulations.
Additionally, high-performance matrix operations are now a core part of the solver. Thanks to the integration of an advanced matrix library, the solver can handle large models more efficiently, resulting in notably faster simulations, especially for multi-physics models with complex structures or numerous state variables. These enhancements are now the default settings in version 2410, streamlining the user experience.
Performance benchmarks
Across various applications, Simcenter Amesim 2410 outshines its predecessor version as well as competitors solving times. The following are some of the most impressive gains observed:
Acceleration made tangible
In developing software like Simcenter Amesim, we use automated test protocols to make sure everything works smoothly and accurately, and to test large number of scenarios simultaneously. The results of these tests are shown in the paragraphs above. While these tests are crucial and offer impressive results, it’s nice to make the difference as tangible as possible to fully see the value of this improvement.
To give you a clear picture, we did a 1:1 comparison, which you can check out in the video below. This side-by-side look really highlights how much faster the new version runs. The actual simulation times can vary based on your specific setup and hardware, but in this example you see the difference when exactly the same demo model is run on the same machine, both in Simcenter Amesim 2404 and Simcenter Amesim 2410.
Imagine the impact of saving 66% on your simulation time with Simcenter Amesim. If you frequently use the software, this isn’t just a minor improvement—it’s a game changer. For instance, in the same time it used to take to run one simulation, you can now run three. This means you can explore more design variations, optimize your models more thoroughly, and ultimately get your projects done faster. But it’s not all work and no play. With the extra time, you could catch up on your favorite show, enjoy a longer coffee break, or even take a quick walk to clear your mind. The possibilities are endless, and the time you save is yours to use however you like.
Conclusion
Simcenter Amesim 2410 brings unprecedented speed and performance gains to system simulation, enabling engineers to tackle complex, large-scale models with greater efficiency. As an example of the value fast simulation can bring, Sub-Zero Group utilized Simcenter Amesim to significantly reduce product development time for its high-end refrigerators. By leveraging 1D simulations, Sub-Zero lowered computational costs and eliminated the need for physical prototypes, allowing the company to efficiently evaluate energy consumption and optimize refrigeration systems.
Simcenter Amesim was so effective that Sub-Zero expects to have its design exploration time reduced from two months to one week, a decrease of 88 percent.
Anderson Bortoletto, Principal Engineer, Advanced Product Development , Sub-Zero Group
The new solver algorithms, combined with optimized matrix operations, allow for simulation acceleration across various use cases. Whether in aerospace, automotive, energy, or industrial applications, Simcenter Amesim 2410 offers a powerful toolset for engineers facing today’s electrification and system simulation challenges. With performance improvements of up to 75% in some cases, of 35% on average and with no regression on the results, this version empowers users to achieve more in less time.
More features released in Simcenter Amesim 2410 are described in this blogpost.