Products

What’s new in Simcenter STAR-CCM+ 2506?

Render photorealistic visuals faster. Speed up design optimization. Mesh complex assemblies efficiently. Simulate bending structures quickly. And more.

The latest release of Simcenter STAR-CCM+ 2506 delivers significant enhancements across CFD simulation workflows, enabling you to tackle complex problems with greater efficiency. With improved performance in meshing, solver technology, and new visualization capabilities, users will experience easier set-up, higher accuracy, faster simulations, and compelling results representations. The release introduces GPU acceleration for particle simulations and photorealistic rendering, enhanced bending capabilities for structural analyses of valves, and improved contact modeling for manufacturing applications like blow-molding. New features like voltage-driven solid coils for electric machine simulation and efficient gear system configuration in conjunction with Smooth Particle Hydrodynamics (SPH) expand Simcenter STAR-CCM+ applicability across industries. Optimized algorithms for surface remeshing and thin parts meshing ensure more robust and faster convergence for challenging geometries.

Learn how to use Support Center

New enhancements in Simcenter STAR-CCM+ are aimed at helping you:

Model applications such as blow molding or film, sheet extrusion with Simcenter STAR-CCM+ 2506

Model the complexity

Unlock higher fidelity and flexibility for e-machines analyses

Engineers working with electric machines often struggle with accurately modeling current density redistribution through solid coil cross-sections, leading to less accurate performance predictions. With the latest release of Simcenter STAR-CCM+ 2506, you can now utilize a new dedicated excitation coil model specifically designed to simulate voltage-driven solid conductors. This approach provides higher fidelity and better usability of both the Finite Element and Harmonic Balance Finite Element Magnetic Vector potential solvers. The new capability allows voltage-driven solid conductors to be modeled natively in both time and frequency domains, eliminating previous limitations. This enhancement enables you to simulate a whole new family of electromagnetic analyses in e-machines, delivering more accurate predictions of performance and efficiency.

Dive deeper into the latest electromagnetic simulation capabilities

Simulate bending structures up to 7x faster

Standard linear hex elements are known to be too stiff in bending deformation, exhibiting the “locking” effect that requires more expensive element formulations. The latest version of Simcenter STAR-CCM+ introduces enhanced linear hex elements that provide the accuracy of quadratic elements at the computational cost of linear elements. You can now experience up to 7x faster simulation of thin structures with bending deformation, as demonstrated in a structure-only simulation with 83,282 elements. This advancement is particularly valuable for applications involving thin-walled components under bending loads, such as sheet metal parts, thin structural members, and lightweight designs. The enhanced formulation maintains accuracy while significantly reducing computational requirements, allowing for more design iterations and larger models within the same computational budget.

Optimize complex manufacturing processes with advanced contact modeling

Manufacturing processes like blow molding or film/sheet extrusion often involve components constrained or manipulated by adjacent parts, making accurate simulation impossible without contact modeling. Simcenter STAR-CCM+ 2506 introduces contact modeling with unmeshed constraining geometry parts for the viscous flow solver, opening possibilities for detailed simulations of a whole new category of manufacturing applications. You can now define constraining geometry parts as stationary or moving via rigid body motion, with walls that may be slip, partial slip, or no-slip. The free surface may contact and be constrained by parts, allowing for realistic simulation of complex manufacturing processes. This advancement enables engineers to accurately predict material behavior during forming processes, leading to optimized designs and reduced physical prototyping.

Improve meshing of thin parts for faster convergence

Quality meshing of thin structures is critical to simulation convergence for many applications, and has traditionally been challenging to achieve efficiently. The latest release of Simcenter STAR-CCM+ 2506 features a new thin volume mesher designed to enhance detection and handling of thin geometries throughout the computational domain. You can now generate meshes where a larger percentage of the overall volume is filled with thin prisms, with improved treatment of stacked thin sections. The enhanced algorithm provides improved transition between thin layer and unstructured meshes, with curve segments now fully compatible. These improvements result in higher-quality meshes for thin structures, leading to faster convergence and more accurate results for applications involving heat exchangers, electronic components, sheet metal parts, and other geometries with thin features. The enhanced meshing capabilities reduce the need for manual mesh adjustments, streamlining the overall simulation workflow.

Learn about how the thin mesher is a key enabler for our customers

Simcenter STAR-CCM+ 2506 hero visual

Explore the possibilities

Accelerate design optimization for discretized geometries

Engineers often struggle with the tedious setup process of surface morphing for shape optimization based on field functions. The latest Simcenter STAR-CCM+ 2506 release addresses this challenge by extending the Morph Surface Mesh Operation with a new Parametric Morphing option. You can now leverage a seamless workflow between the parametric surface morpher and Design Manager, enabling reliable morphing of any tessellated input geometry through user-defined vector parameters in cartesian directions. This enhancement significantly accelerates the design optimization process for discretized geometries.

Explore about design optimization

Inter-continuum partitioning, with Simcenter STAR-CCM+ 2506

Go faster

Create photorealistic imagery quickly with powerful GPU-accelerated rendering

Creating photorealistic digital twin representations with simulation results has traditionally been very time-consuming, requiring specialized expertise. The new Studio Scene feature in Simcenter STAR-CCM+ 2506 enables effortless photorealism with an intuitive workflow and GPU-accelerated ray tracing. You can now experience the democratization of photorealism with real-time view interaction, making high-quality visualization accessible to all users. The feature provides automatic and workflow-aware defaults that reduce overall setup time, along with an interactive workflow to create, assign, and change photorealistic rendering materials. Supported for any NVIDIA RTX line GPU, this capability delivers up to 11 times faster rendering compared to CPU-based methods. Photorealistic hardcopies can be created while the simulation is running, enabling you to produce compelling visualizations for presentations and reports with minimal effort.

Run faster Conjugate Heat Transfer (CHT) simulations

The exchange of information at contact interfaces between fluid and solid domains has traditionally impacted simulation performance due to suboptimal partitioning strategies. The latest version of Simcenter STAR-CCM+ introduces a new partitioning method called Inter-Continuum partitioning, specifically optimized for interactions between fluid and solid continua. You can now experience faster performance for simulations with multiple continua such as conjugate heat transfer, with benefits for both contact and mapped contact interfaces on both CPUs and GPUs. Performance improvements are substantial, with speed-ups of 21% for a cooled turbine blade case on 4 GPUs, 52% for a sports car vehicle thermal management simulation on 12 GPUs, and 12% for a transient battery thermal simulation on 320 CPU cores. These enhancements make Simcenter STAR-CCM+ 2506 significantly more efficient for thermal management applications across industries.

Explore GPU-accelerated CHT simulations

Accelerate mesh generation

The concurrent meshing of geometries with substantial size differences can result in suboptimal scaling, creating a bottleneck in preprocessing workflows. With Simcenter STAR-CCM+ 2506, you can now leverage the new Concurrent-parallel per-part meshing mode that intelligently accounts for part sizes in process assignment. This enhancement delivers up to 2.15x speedup between concurrent and concurrent-parallel modes, making more efficient use of available computational resources. You’ll experience faster mesh generation while maintaining consistent mesh quality with serial execution. This improvement is particularly beneficial for complex assemblies with components of varying sizes and complexity, allowing for more efficient preprocessing and faster overall simulation turnaround times.

Speed up surface meshing

To speed up end-to-end simulation pipelines, every step including surface remeshing must contribute to overall efficiency gains. Simcenter STAR-CCM+ 2506 delivers enhanced Surface Remesher capabilities that provide faster surface remeshing on a single processor. You can now experience up to 40% reduction in surface remeshing time depending on case complexity, without requiring any additional input to enable the feature. This improvement is particularly valuable for workflows involving multiple remeshing operations or large, complex geometries. With Simcenter STAR-CCM+ 2506’s reduced surface preparation time, engineers can shift their focus from preprocessing tasks to valuable analysis and design improvements.

Learn how to mesh faster with the Surface Remesher

Run LES combustion up to 20% faster with PISOC

Large Eddy Simulation (LES) approaches for unsteady combustion simulations demand substantial computational resources and lengthy calculation periods. Simcenter STAR-CCM+ 2506 introduces the PISO-Consistent (PISOC) implicit scheme for the Segregated Flow solver, designed to speed up these demanding simulations. Similar to SIMPLEC, no relaxation is applied to the pressure equation, allowing for deeper convergence of the PISO residual. You can now achieve faster solve times per time step as the scheme requires fewer correctors. Testing on an industrial gas combustor with 51 million cells using LES (WALE) and FGM approaches shows up to 20% faster simulation times. This enhancement significantly improves productivity for engineers working on combustion applications, allowing for more design iterations within project timelines.

Read how SIMPLEC improves CFD efficiency

Run DEM analysis with GPU-native solver

Particle simulations with Meshfree DEM have traditionally been limited to CPU-based solvers, restricting simulation size and speed. Simcenter STAR-CCM+ 2506 introduces a GPU-native Meshfree DEM solver that delivers faster turnaround times and more energy and cost-efficient simulations for a wide range of applications involving particle flow. You can now run these simulations on GPUs while maintaining equivalent solutions between CPU and GPU implementations.

GPU-native Meshfree DEM with Simcenter STAR-CCM+ 2506

The GPU-native DEM is fully compatible with rigid body motions and DFBI (Dynamic Fluid Body Interaction), ensuring versatility across application areas. This release marks the first step in porting all DEM features to GPU, beginning with support for spherical particle types. With less costly simulation, you can tackle larger particle systems or run more design iterations within the same timeframe, leading to optimized designs for applications like bulk materials handling and solids mixing.

Watch Discrete Element Method at a glance

More accurate and more data analysis with Simcenter STAR-CCM+ 2506

Stay integrated

Extend simulation insight to the enterprise digital thread

Managing simulation data within PLM systems has traditionally been challenging due to the massive file sizes involved. With the new release of Simcenter STAR-CCM+, you can now directly visualize simulation files (.sce) in Teamcenter without checking in large datasets. The solution enables quick results upload to Teamcenter and includes comprehensive visualization options such as histograms, time history plots, bubble charts, and heat maps within your CAE 3D models. This seamless integration maintains the digital thread between CAE experts and the PLM system while significantly reducing data management overhead.

Learn more about Simcenter STAR-CCM+ integration with Teamcenter

Streamline gear systems setup with automated kinematics

Setting up gear systems simulations has traditionally required manual calculation and application of individual component kinematics, leading to labor-intensive setup processes and increased risk of errors. Simcenter STAR-CCM+ 2506 introduces an efficient configuration approach for gear systems through the new DFBI motion Kinematics Solver and specialized joints. You can now achieve quick and easy motion coupling for gears, eliminating the need for complex manual calculations and setup. This new capability is compatible with SPH and Finite Volume methodologies, making it versatile across different simulation approaches. Applications include gearbox and differential lubrication, ball-bearing simulation, rotorcraft transmissions, and many other mechanical systems. The result is significantly easier and more efficient setup of gear systems simulations, allowing you to focus on analysis rather than model configuration.

Maximize simulation performance with enhanced SPH capabilities

In today’s demanding engineering environment, computational fluid dynamics (CFD) simulations often face challenges with accuracy, processing time, and complex setup procedures. With the release of Simcenter STAR-CCM+ 2506, you can now leverage significantly enhanced Smoothed Particle Hydrodynamics (SPH) capabilities that address these critical challenges head-on. You’ll experience increased accuracy in run-off applications and torque predictions, along with improved free surface rendering that delivers more realistic results. The new release streamlines your workflow with enhanced motion setup features, including reference frame capabilities for rotating inlet boundary conditions and efficient gear system simulation setup. When it comes to performance, the results are significant – you can achieve up to 25% faster turnaround time and benefit from up to 3 times faster initialization through optimized ghost particle generation. These improvements are demonstrated in benchmarks using NVIDIA A100 GPU, where Simcenter STAR-CCM+ 2506 release shows significant performance gains over its predecessor. With these comprehensive enhancements, you can now focus more on innovation and less on computational overhead, ultimately delivering better designs in less time.

Explore how SPH enhancements accelerate CFD


These are just a few highlights in Simcenter STAR-CCM+ 2506. These features will enable you to design better products faster than ever, turning today’s engineering complexity into a competitive advantage.

Read Simcenter STAR-CCM+ reviews on G2
Bahaa Haddoukessouni
Lead Product Manager, Simcenter STAR-CCM+

Bahaa Haddoukessouni is the Product Management team leader for Simcenter STAR-CCM+, where she leads her team in shaping the product strategy and roadmap to facilitate faster engineering and innovative product development for customers. With 18 years of experience in simulation, she is dedicated to understanding market challenges and addressing customer needs. By collaborating closely with cross-functional teams such as development, sales, and support, Bahaa and her team ensure the delivery of customized CFD and integrated Multiphysics solutions to accelerate product development and drive digital transformation initiatives effectively.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/simcenter-star-ccm-2506-released/