It’s hard to believe that the Design Automation Conference (DAC) is coming up in less than two weeks. As always,…
I’m really excited to share with you a very special issue of the Verification Horizons newsletter for September, 2021. The…
ISO26262 remains the state-of-the-art standard governing the activities required to prove electronics and electronic systems are safe for deployment in…
It’s likely no surprise that EV, ADAS, and AV applications are driving a new level of complexity in the planning,…
IC complexity for automotive applications continues to grow with experts estimating that automotive electronics will eventually exceed 50% of total…