Thought Leadership

Part 5: The 2010 Wilson Research Group Functional Verification Study

Effort Spent On Verification (Continued)

This blog is a continuation of a series of blogs, which present the highlights from the 2010 Wilson Research Group Functional Verification Study.

In my previous blog, I focused on the controversial topic of effort spent in verification. This blog continues this discussion.

I stated in my previous blog that I don’t believe there is a simple answer to the question, “how much effort was spent on verification in your last project.”  I believe that it is necessary to look at multiple data points to truly get a sense of the real effort involved in verification today. So, let’s look at a few additional findings from the study.

Time designers spend in verification

It’s important to note that verification engineers are not the only project members involved in functional verification. Design engineers spend a significant amount of their time in verification too, as shown in Figure 1.

5slide1

Figure 1. Mean time designer spends in design vs. verification

In fact, one finding from our study is that the mean time a design engineer spends in verification has increased from an average of 46 percent in 2007, to 50 percent in 2010. The involvement of designers in verification ranges from:

  • Small sandbox testing to explore various aspects of the implementation
  • Full functional testing of IP blocks and SoC integration
  • Debugging verification problems identified by a separate verification team

Percentage of time verification engineers spend on various task

Next, let’s look at the mean time verification engineers spend on various task related to their specific project. You might note that verification engineers spend most of their time in debugging. Ideally, if all the tasks were optimized, then you would expect this. Yet, unfortunately, the time spent in debugging can vary significantly from project-to-project, which presents scheduling challenges for managers during a project’s verification planning process.

5slide2

Figure 2. Mean time verification engineers spend in different task

Number of formal analysis, FPGA prototyping, and emulation Engineers

Functional verification is not limited only to simulation-based techniques. Hence, it’s important to gather data related to other functional verification techniques, such as the number of verification engineers involved in formal analysis, FPGA prototyping, and emulation.

Figure 3 presents the trends in terms of number of verification engineers focused on formal analysis. In 2007, the median number of verification engineers focused on formal analysis on a project was 1.68, while in 2010 the median number increased to 1.84.

5slide3

Figure 3. Median number of verification engineers focused on formal analysis

Figure 4 presents the trends in terms of number of verification engineers focused on FPGA prototyping. In 2007, the median number of verification engineers focused on FPGA prototyping on a project was 1.42, while in 2010 the median number increased to 2.04. Although FPGA prototyping is a common technique used to create platforms for software development, it can be used for SoC integration verification and system validation.

5slide4

Figure 4. Number of verification engineers focused on FPGA prototyping

Figure 5 presents the trends in terms of number of verification engineers focused on hardware assisted acceleration and emulation. In 2007, the median number of verification engineers focused on hardware assisted acceleration and emulation on a project was 1.31, while in 2010 the median number increased to 1.86.

5slide5

Figure 5. Number of verification engineers focused on emulation

A few more thoughts on verification effort

So, can I conclusively state that 70 percent of a project’s effort is spent in verification today?  No.  In fact, even after reviewing the data on different aspects of today’s verification process, I would still find it difficult to state quantitatively what the effort is. Yet, the data that I’ve presented so far seems to indicate that the effort (whatever it is) is increasing. And there is still additional data relevant to the verification effort discussion that I plan to present in upcoming blogs. However, in my next blog I shift the discussion from verification effort, and focus on some of the 2010 Wilson Research Group findings related to testbench characteristics and simulation strategies.

Harry Foster
Chief Scientist Verification

Harry Foster is Chief Scientist Verification for Siemens Digital Industries Software; and is the Co-Founder and Executive Editor for the Verification Academy. Harry served as the 2021 Design Automation Conference General Chair, and is currently serving as a Past Chair. Harry is the recipient of the Accellera Technical Excellence Award for his contributions to developing industry standards. In addition, Harry is the recipient of the 2022 ACM Distinguished Service Award, and the 2022 IEEE CEDA Outstanding Service Award.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2011/04/04/part-5-the-2010-wilson-research-group-functional-verification-study/