This post introduces the most common and sought after use of automation in Solid Edge – creating and controlling Parametric Parts via an external program.
Using the Solid Edge API it is ea…
Using 3D scanned data to create parts with complex shapes is some of the most difficult work I’ve ever done. So I attended this session at Solid Edge University. Ricardo Espinosa from Kimball Interna…
If you work with imported data from any source, Solid Edge Synchronous Technology is the tool you need to be using. In this Solid Edge University presentation, Chris Dayton of the Solid Edge planning…
Here is another presentation that I gave at Solid Edge University this year. This one goes through the surfacing features of a bottle and a bobsled type shape to show how to create a smooth shape whe…
In this Solid Edge University session, Craig Ruchti, from field support, leads a hands-on session leading users through using features in mixed Ordered and Synchronous modes. Craig advocates changing…
This is just for fun but not simply icon guessing, If you have a clue icon for Physical properties, the word could be Physical, Properties, Mass, Volume, Area, Density, Material, etc.
…
This was the first session I attended at Solid Edge University this year. Rahul Kulkarni presents the functionality of 3D Sketch as added to ST7. This is an important tool, since you can use it in ma…
Karsten Newbury gave the kickoff speech, and gave a business update with some numbers folks aren’t used to seeing from Solid Edge. Maybe you weren’t there this year, and want to see what you missed, …
One of the biggest challenges of automating Solid Edge (for me at least) is the sheer size of the API. SDK documentation and examples are nice but these are static views of the API. What wou…