New Tech Tip describes new-for-NX CAM 9 Cut Region Management

Last week’s Tech Tip was the first in our series of new NX CAM 9 enhancement webinars. This Tech Tip describes some powerful new options for optimizing cut patterns across steep and non-steep regions…

NX CAM 9 preview: Take precise control over die-mold machining strategies

 
Cut Region Management is one the many new capabilities in NX CAM 9 for die-mold machining. With Cut Region Management, you get precise control over area milling cut regions and machinin…

NX CAM 9: Providing industrial-strength CAM for die/mold machining

NX TM CAM 9 software is available now, and it offers industrial strength CAM for a wide range of industries. If you’re a manufacturer looking for the next level of control and faster CNC progr…

Pencil Milling Part 2

In this post, I want to explain some of the options for working with Flow Cut.  I find that new users consistently struggle with understanding some of these options.

First up is Max…

Pencil Milling Part 1

“Pencil Milling” is the name given to a machining strategy where a small-diameter ball end mill is used to perform finish milling in small nooks and crannies of a complex mold or die.  The word …

Machining Steep and Non-steep Geometry (Part 2)

In my last post, I showed several wrong ways to machine steep and non-steep geometry.  In this post, I will show a method that is better.

NX CAM can scrutinize a model and determine…

Tool Path Divide

  If you really want to scare an NC programmer, just show them a deep, narrow cavity on your latest design, and then comment that you must have a mirror-like surface finish at the bottom. …

Roughing and Re-roughing

In NX CAM we refer to a specific set of machining instructions as an operation.  For example, finish-milling a planar face would be one operation.  To spotdrill, drill, and bore a hole requ…

The Evolution of Tool Path Design (Part 3)

In this post, I will explain the latest tool path innovations for removing large quantities of material.I mentioned in Part 2 that Offset tool paths have problems when the offsets meet at shar…