4 Simcenter Presentations at the Shock and Vibration Symposium 2022
Attention structural dynamics and vibrations engineers – the 92nd Shock and Vibration Symposium is coming up on September 18-22, 2022 in Denver, Colorado USA. Organized by the Shock and Vibration Exchange (SAVE), this event, established in 1947, is the leading forum for engineers in the structural dynamics and vibration community to present and discuss new developments and ongoing research.
Simcenter, from Siemens Digital Industries Software, a leader in vibrations engineering for decades, is proud to be presenting four papers at the Shock and Vibration Symposium:

Wednesday, September 21
Multiple-Input Multiple-Output acoustic testing of turboprop fuselage structures
Learn how Siemens and its partners have developed a faster and cheaper approach for helping to cut the noise inside turboprop cabins by reducing the need for expensive and time-consuming flight tests or low noise wind tunnel tests. Instead, a near-field array of loudspeakers can be used to synthesize a pressure field on the fuselage surface similar to the loads generated by both the turbulent boundary layer and the propeller blade passages, simultaneously.

Wednesday, September 21
Monitoring of Virtual Full-Field responses during Direct Field Acoustic Noise (DFAN) environmental acoustic tests
Learn how the space industry is reducing cost and risk over standard environmental acoustic test processes. Instead of performing tests in expensive, large reverberant chambers, the space industry is moving towards more use of the Direct Field Acoustic Noise (DFAN) test method. However, it can be difficult for engineers to truly understand what is happening with the system during a test. Simulation can help overcome this problem, and this paper will show how a full multi-physics model, which simulates the electro-acoustic frequency response functions (FRFs) of the physical test system, is directly accessible online during the DFAN test. Engineers can update the simulation model onsite using the experimental FRFs obtained in the system identification step. Using simulation in connection with test helps engineers gain insight into certain physical phenomena which are difficult to foresee based on the observations at a limited number of sensors

Thursday, September 22
Simultaneous control of multiple strain responses in MIMO Random vibration control tests
Over the last decade, engineers have brought laboratory testing conditions closer to replicating the in-service operational environment through the use of Multi-Input Multi-Output (MIMO) random vibration control. To help make lab test even more closely resemble the real world, this paper will cover a new unexplored possibility in the MIMO random control testing practice: the simultaneous control of multiple strain responses instead of traditional accelerations.

Thursday, September 22
Latest software and hardware developments enabling enhanced replication of MIMO Random vibration environments
Although Multi-Input Multi-Output (MIMO) control has been in existence since 1958, it has widely been seen as too complex and only began getting traction with the test engineering community in the early 2000’s. The objective of this presentation is to give a detailed insight on how software and hardware advancements in recent years in MIMO control technology help realistically reproduce random vibration environments that products experience during operation while also overcoming the stigma of overcomplex testing practices.
Hands-on Learning
Not only can you listen to papers, but you can also use your time to get valuable hands-on learning at the Shock and Vibration Symposium. Siemens will be giving a tutorial on the following topic at this event:
Fundamentals of Classic Shock and SRS Shake Testing
This tutorial will cover the fundamental concepts of shaker shock testing, from field data acquisition to Classic Shock and Shock Response Spectrum (SRS) wavelet synthesis in a vibration controller. The tutorial will cover shock data acquisition and processing, along with a segment addressing the sensors used for this application. See live demos of data acquisition and shaker tests and get hands-on opportunities to try out the tools.
Visit the Siemens booth
In addition to these exciting papers and tutorial, you can stop by the Siemens booth where you can talk directly with our engineers about the technology presented in the sessions, as well as see up close a demo of MIMO closed loop control with strain gages.
Register today
If you’re a structural dynamics and vibrations engineer, you won’t want to miss this event. You can see the full agenda and register for the event by clicking the buttons below:
We look forward to seeing you there!