Corporate

How the AI CSP generator helps partners win more renewals faster

Most partners know they should have a customer success plan. Very few actually do. Not because they don’t see the value, but because building a quality CSP takes time nobody thinks they have. When the choice is between writing documentation and working an active deal, the documentation loses every time.

That tradeoff has real consequences. Renewals stall without a clear value narrative. Expansion conversations lack the evidence to move forward. And when an executive asks what’s been delivered, there’s nothing prepared to show them.

We built the AI-assisted CSP Generator to address that directly. Not to automate the relationship, but to handle the structural work so partners can focus on the conversations that actually require their judgment.

The pattern shows up consistently across partner accounts. CSP creation gets deprioritized not because anyone disagrees with its importance, but because the work feels disproportionate to the moment. A partner managing 20 active accounts isn’t skipping CSPs out of laziness. They’re making a capacity call, and the plan loses to the pipeline.

The result plays out predictably:

  • Renewal conversations start from scratch instead of from a documented baseline
  • Adoption gaps surface late, when there’s less time to act
  • Expansion opportunities get missed because there’s no structured record of what the customer actually achieved
  • Executive conversations lack the concise narrative that leadership needs

A plan that never gets written can’t help anyone.

The problem is partners don’t know how to build a CSP.  The issue is they create them, when they do based on features and functions. Not pulling together customer context, structuring outcomes, framing the value story. That’s exactly where momentum dies. Traditional approaches either produce something too thin to be useful, or require so much effort that the standard slips when things get busy.

That’s what we designed around.

What the CSP generator actually is

The AI-assisted CSP Generator is a guided workflow built inside the Siemens Xcelerator SiemensGPT Partner Workspace. It takes structured inputs and produces a complete, customer-ready success plan without requiring hours of document drafting.

Partners start by selecting an account and gathering the relevant context:

  • Customer industry, solutions and business unit
  • Key stakeholders and executive sponsors
  • User count, key dates and renewal timeline
  • Goals, challenges and desired outcomes

The tool works through staged drafting with approval gates between sections. Each gate is a real checkpoint. The quality of the output depends on the accuracy of what gets approved, so the process is designed to slow partners down at the right moments rather than rush them to a finished document.

Why this matters for sellers

A well-structured CSP gives partners a documented reason to be in the room at renewal, not just a date on a calendar.

When a customer can see a clear record of what was committed, what was delivered and what comes next, the renewal conversation shifts. It moves from a pricing discussion to a value review. That’s a fundamentally different dynamic, and partners who operate with that kind of consistency tend to win more often.

The same logic applies to expansion. The hardest part of a growth conversation is proving the baseline worked. A CSP maintained across the engagement makes that proof straightforward. It also reduces the discount pressure that fills the gap when evidence isn’t available.

Practical ways partners can use it

Upcoming renewals. Start with an account at least 120 days out so the CSP is ready 90 days out. Use the generator to work with your customer and build the plan now, while there’s still time to act on any gaps it surfaces.

Adoption risk accounts. For customers showing low engagement or limited utilization, the CSP structure forces the right questions early, before the renewal conversation becomes a recovery conversation.

Expansion-ready accounts. When an account is ready for a growth conversation, a completed CSP provides the evidence base. It moves the discussion from aspiration to documentation.

New accounts. Starting a CSP at onboarding sets the standard for the entire relationship. It signals to the customer that outcomes are being tracked, not assumed.

A standout capability worth noting

The output package includes more than one document. Depending on configuration, the generator produces a detailed customer-facing CSP, a working Excel file for ongoing tracking, a source and assumptions appendix, and a concise executive summary formatted for leadership audiences.

That last piece matters more than it might look. Partners frequently lose traction not because the account relationship is weak, but because the executive narrative isn’t ready when it’s needed. A formatted executive document as a standard deliverable removes that gap entirely.

A simple way to get started

Pick one account, not your most complex. Choose something real: a renewal coming up, an account with adoption questions, or one that’s ready for an expansion conversation.

  • Log in to SiemensGPT and open the CSP Generator in the Partner Workspace
  • Gather the customer inputs before you start: industry, stakeholders, goals and key dates
  • Work through each approval gate deliberately and only advance when the content is directionally correct
  • Review every assumption the tool flags and confirm or correct it before moving forward
  • Generate the output package and use the executive document in your next customer touchpoint

The goal is one completed CSP on a real account within 30 days. Everything builds from there.

Partners who consistently outperform over the next few years won’t be the ones working harder on individual deals. They’ll be the ones building operating models that scale. Structured customer success planning is part of that model. It’s what separates partners who hold accounts from partners who grow them.

The CSP Generator doesn’t replace the relationship. It makes the relationship defensible.

Not yet certified? Complete the SiemensGPT certification to get access to the Partner Workspace.

Already certified? Open the CSP Generator and run your first plan on a real account. Aim to have one completed CSP within 30 days.

Want to learn more? Access the enablement deck for a full walkthrough of the CSP Generator and how to get the most out of it.

About the authors

Benedict Russell is a Global Partner Development Executive responsible for scaling global GTM programs across all motions. He helps shape Siemens’ digital selling and AI strategy, embedding best practices that accelerate SaaS adoption and recurring revenue. Previously, he drove partner coverage and expansion, adding 300+ partners to the Siemens ecosystem.

William McInnis is a Global Partner Development Executive at Siemens Digital Industries Software, where he focuses on global go-to-market programs, partner operations strategy, customer success, renewals, and Siemens’ XaaS transformation. With more than 25 years of experience across Accenture, Lockheed Martin, Microsoft, Autodesk, and Siemens, William has led global programs spanning customer success, cloud adoption, solution delivery, business integration, and enterprise transformation. He is especially focused on helping partners adopt LAER-based customer engagement practices that improve customer outcomes, renewal performance, and sustainable growth.

Benedict Russell

Bill McInnis

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/partners/ai-customer-success-plan-generator/