Thought Leadership

A Little Verilog Knowledge Goes A Long Way in Understanding How SystemVerilog Constraints Work

In its simplest form, a constraint is nothing more than a Boolean expression with random variables where the solver is asked to find values that make the expression true. One way of thinking about how a constraint solver works is that it repeatedly tries different values until the values make the expression true, then it writes those values into the set of random variables. It’s actually much more complicated than that because we want the solver to quickly converge on a solution or tell us no solution is possible without wasting a lot of time. But let’s just focus on the expression evaluation.

A fundamental principle that drove SystemVerilog’s development was unifying semantics so that expression evaluation was identical across all facets of the language. This meant all the idiosyncrasies from Verilog’s weak type and expression evaluation systems got absorbed into constraint expressions. One of the unique things that distinguishes Verilog from most other programming languages is its ability to declare variables of different bit-widths and have expressions of mixed bit-widths. The weak type system means it silently truncates and pads different bit widths without any notice of overflow or underflow. This system also has to deal with signed and unsigned arithmetic, and real to integer truncation.

Let’s look at the following two seemingly equivalent expressions:

Expression A: (X * 4) == Y

Expression B:  X == (Y /4)

If we remember our elementary algebra, the division property of equality says we should be able to divide both sides of the equality in Expression A by 4 and wind up with Expression B. You would think using either expression in a constraint gives the exact same results. NOT TRUE. Each expression has a complex series of steps for determining the bit width of an expression result and all the intermediate operations. We need to be aware of this even when we think everything has the same bit-widths.

For Expression A, suppose we declared X and Y as 32-bit unsigned variables (the numeric literal 4 is also considered 32-bits. Verilog has a table for every operator that specifies the resulting width its result. For all arithmetic operators the result width is the size of its largest operand, not the width of the largest possible result which would be 34 bits in this case. This means the result of 32’h40000001*32’d4 gets truncated to 32’h00000004. So, the solver could choose either 32’h40000001 or 32’h00000001 for X when choosing the value 32'h00000004 for Y.

The solution space for (X * 32'd4) == Yis shown in the following table.

X Y
32'h00000000 32'h00000000
32'h00000001 32'h00000004
32'h00000002 32'h00000008
32’h3FFFFFFF 32'hFFFFFFFC
32'h40000000 32'h00000000
32'h40000001 32'h00000004
32’hFFFFFFFF 32'hFFFFFFFC

 

The fix for this is making sure the width of the multiplication result is large enough not to truncate using : (X * 34’d4) == Y. That eliminates the overflow truncation and the second set of unexpected solutions.

For expression B, the bit-widths are not as precarious.  But we do need to understand Verilog integer division truncates any fractional part towards 0, it does not round. That means there will be for consecutive values for Y associated with one value of X. The solution space for X == (Y / 4) is shown in the following table.

X Y
32'h00000000 32'h00000000
32'h00000000 32'h00000001
32'h00000000 32'h00000002
32’h00000000 32'h00000003
32'h40000001 32'h00000004
32'h40000001 32'h00000005
32’h3FFFFFFF 32'hFFFFFFFF

 

To summarize, I’ve show a simple example of how Verilog expression evaluation rules affect the solution space of your SystemVerilog constraints. So anytime you get unexpected values from the constraint solver, go back to your textbooks on Verilog or even Algebra to remember how expressions get evaluated.

Dave Rich

Dave Rich is Verification Technologist at Mentor Graphics and is one of the authors of Mentor’s Advanced Verification Methodology cookbook. He began his career as a design and verification engineer in 1981 at Data General. In 1987, he joined Gateway Design Automation as one of the first application engineers to support Verilog-XL. At Gateway, he helped design many of the early features of the Verilog Hardware Description Language (HDL), and after Cadence acquired Gateway, helped prepare the Language Reference Manual (LRM) that would eventually be donated to the newly formed Open Verilog International. In 1995, he joined another Verilog simulation company, Frontline Design Automation as an AE manager and later as a Product Manager after it was acquired by Avant!. In 1998, he joined Ambit Design and worked as a consulting engineer for both synthesis and simulation products after it was acquired by Cadence. In 2000, he joined Co-Design Automation as Director of Application Engineering where the Superlog HDL was being developed that eventually became the basis of the Accellera SystemVerilog 3.0 standard. Co-Design Automation was acquired by Synopsys in 2002. Dave began work on numerous technical committees within Accellera and later the IEEE P1800 working group, which he continues today.

More from this author

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2019/09/12/verilog-in-constraints/