Thought Leadership

Unlocking the Future of High Bandwidth Memory with Siemens and Rambus

In a recent webinar, Siemens partnered with Rambus to delve into the transformative world of High Bandwidth Memory (HBM), focusing on the latest advancements with HBM4.  This session was a treasure trove of insights for anyone involved in AI, machine learning, and high-performance computing, showcasing how HBM4 is set to revolutionize these fields by significantly boosting data transfer speeds and alleviating performance bottlenecks.

What’s New in HBM4?

HBM4, the next-generation memory technology, is nearing finalization by JEDEC and promises to push the boundaries of data rate, 3D stack height, and DRAM chip density.  This evolution from HBM3 to HBM4 means even higher bandwidth and greater device capacity, making it indispensable for the growing demands of AI and HPC applications.  Key highlights include:

  • Increased Data Rate: HBM4 supports data rates up to 9.6 Gbps per pin, significantly higher than its predecessors.  This increase in data rate allows for faster processing and more efficient handling of large datasets.
  • Higher Capacity: With up to 64GB per stack, HBM4 can handle massive datasets efficiently.  This higher capacity is crucial for applications that require extensive memory resources, such as AI training and high-performance computing.
  • Enhanced Energy Efficiency: Optimized power-to-bandwidth ratio, ideal for large-scale computing needs.  This improvement helps reduce overall power consumption, making systems more sustainable and cost-effective.

What You Will Learn

The webinar provided a comprehensive overview of the challenges and innovations in verifying advanced HBM generations.  Attendees learned about:

  • Verification Challenges: The complexities involved in verifying HBM4 and how Siemens’ Avery HBM Verification IP addresses these challenges.  Understanding these challenges is essential to ensure the reliability and performance of HBM4-based systems.
  • Unique Features: The distinctive features of Siemens’ HBM4 memory models ensure reliability and performance.  These features include advanced error correction and high-speed data transfer capabilities.
  • Rambus’s HBM4 Controller IP: Insights into Rambus’s newly announced HBM4 memory controller IP and its positive impact for the industry.  This controller IP is designed to maximize the performance and efficiency of HBM4 memory systems.

Who Should Watch the Recording?

This webinar is a must-watch for:

  • Design & Verification Engineers: Gain deep insights into the latest verification techniques and tools. These insights can help engineers improve their design processes and ensure the success of their projects.
  • Architects: Understand the architectural advancements and how they can be leveraged in your designs.  This knowledge is crucial to create efficient and high-performance systems.
  • Managers and Directors: Learn about the strategic benefits of adopting HBM4 technology and how it can drive your projects forward.  This information can help you make informed decisions about technology investments and project planning.

Watch the Recorded Webinar

To dive deeper into the world of HBM4 and see how Siemens is supporting designs using this cutting-edge technology, watch the full webinar recording here.  Discover how Siemens’ scalable and customizable Avery HBM Verification IP helps companies like Rambus verify their industry-leading HBM4 Controller IP through rigorous testing to ensure reliability and performance.

Stay ahead of the curve with Siemens and Rambus to unlock the full potential of High Bandwidth Memory in your next project.

Dennis Brophy
Director of Ecosystems

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/verificationhorizons/2024/11/05/unlocking-the-future-of-high-bandwidth-memory-with-siemens-and-rambus/