Products

Logistics Planning in Universities? Material Flow Simulation for Students?

The Plant Simulation Student Challenge starts into round two: Solve our electric motor final assembly task! Join the Tecnomatix Plant Simulation Award with the Chance to Win a Microsoft Surface Touchscreen-Based Computer, a Powerful Bluetooth Wireless Speaker, or a Smart Watch!

The Plant Simulation Student Challenge starts into round two: Solve the electric motor final assembly task!

Plant Simulation Student Award Invitation
Plant Simulation Student Price Invitation

Plant Simulation Challenge

Siemens Digital Industries Software Tecnomatix Plant Simulation is the software for modeling, simulating, analyzing, visualizing, and optimizing of production systems, logistics and processes. You can create a Digital Twin of a process, a production line or even a full factory and develop, enhance, or adjust it to new requirements.

Register for the quarterly challenges now!

Register and solve our given tasks by using Tecnomatix Plant Simulation. Download your free Student Version right here!

Awards:

First place wins a Microsoft Surface touchscreen-based computer!

Second place wins a powerful Bluetooth Wireless Speaker, and third place wins a Smart Watch.

All participants with reasonable solutions will receive a digital badge acknowledging you as a Plant Simulation challenge participant.

Register for the quarterly challenges now!

The solution must be solved with Tecnomatix Plant Simulation.
Anyone outside Siemens Digital Industries Software and its business partners may participate.
Important dates:
Announcement of the task: July 11th, 2022
Deadline for submissions: September 30th, 2022

Discrete Event Simulation in Universities, Accademics, Teaching and Learning

Electric motor final assembly

Plant Simulation Student Award

A major car manufacturer wants to build a new production line for electric motors.

In the final assembly area, three machines and a quality inspection station are connected by conveyor belts.

All conveyor belts have a transportation speed of 1 m/s.

For the first machine (M1), the processing time is 15 seconds.

For the second machine (M2), the processing time is 10 seconds, and this machine may malfunction. The machine M2 has an availability of 88% and a Mean Time to Repair (MTTR) of one minute.

After the machine M2, the material flow is split up, as follows:

90% of the motors go directly to the third machine (M3) and 10% of the motors are moved to the quality inspection station (Q1).

Since the quality inspection time is not yet exactly known and is subject to a manual process. We assume that the time will be equally distributed between one minute and four minutes.

After quality inspection the parts are sent to the machine M3.

The processing time of machine 3 (M3) is 10 seconds.

Questions:

Q1: Compute the average throughput per day of the line.

Q2: Find out the relative occupancy of the quality inspection station.

Q3: Which station is most relevant for the output quantity of the plant?

German: Produktionslinie für Elektromotoren

Ein großer Automobilhersteller möchte eine neue Produktionslinie für Elektromotoren aufbauen.

Im Bereich der Endmontage kommen dazu 3 Maschinen, die über Förderbänder verbunden sind und eine Qualitätssicherung zum Einsatz.

Alle Förderbänder haben eine Transportgeschwindigkeit von 1m/s.

In der ersten Maschine M1 beträgt die Bearbeitungszeit 15 Sekunden.

In der zweiten Maschine M2 beträgt die Bearbeitungszeit 10 Sekunden, in dieser Maschine kann es zu Störungen kommen. Die Maschine M2 hat eine Verfügbarkeit von 88% und eine Mean Time to Repair (MTTR) von einer Minute.

Nach der Maschine M2 teilt sich der Materialfluss auf:

90% der Motoren gehen direkt weiter an die Maschine M3, 10% der Motoren werden zur Qualitätssicherung Q1 ausgeschleust.

Da die Qualitätssicherung noch nicht genau bekannt ist und einem manuellen Prozess unterliegt soll die Zeit für Qualitätssicherung gleichverteilt zwischen einer Minute und vier Minuten angenommen werden.

Auch die Teile nach der Qualitätssicherung werden zu Maschine M3 geschickt.

Die Bearbeitungszeit in der Maschine M3 beträgt 10 Sekunden.

Fragen:

F1: Berechnen Sie die mittlere Ausbringungsmenge der Anlage pro 24 Stunden.

F2: Berechnen sie die relative Belegung in der Qualitätssicherung.

F3: Welche Station ist entscheidend für die Ausbringungsmenge der Anlage?

Chinese

电机装配

一家大型汽车制造商希望建造一条新的电机生产线。

总装区,3台机器和一个质量检测站通过传送带连接。

所有输送带的运输速度均为 1 m/s

对于第一台机器(M1),时间为15秒。

对于第二台机器(M2),时间为10秒,这台机器可能会出现故障。M2 机器的利用率 88%,平均维修时间 MTTR 1 钟。

M2机器之后,物料流被分流如下:

90%电机直接进入第三台机器(M3),10%电机移至质量检测站(Q1)。

由于质量检查时间尚不确切,并且需要手动处理,因此应假定时间将平均分布在一分钟到四分钟之间。

质量检查后的零件被送到M3机器。

机器3M3)中的艺处时间为10秒。

问题:

Q1计算生产线每天的平均量。

Q2计算质检站的相对占用率。

Q3:哪个站与工厂的产量最相关?

France: Assemblage final du moteur électrique

Un grand constructeur automobile veut construire une nouvelle ligne de production de moteurs électriques.

Dans la zone d’assemblage final, 3 machines et un poste de contrôle qualité sont reliés par des bandes transporteuses.

Toutes les bandes transporteuses ont une vitesse de transport de 1 m/s.

Pour la première machine (M1), le temps de traitement est de 15 secondes.

Pour la deuxième machine (M2), le temps de traitement est de 10 secondes et cette machine peut mal fonctionner. La machine M2 a une disponibilité de 88% et un temps moyen de réparation (MTTR) d’une minute.

Après la machine M2, le flux de matière est divisé comme suit :

90% des moteurs vont directement à la troisième machine (M3) et 10% des moteurs sont déplacés vers la station de contrôle qualité (Q1).

Étant donné que le temps d’inspection de la qualité n’est pas encore connu exactement et fait l’objet d’un processus manuel, il convient de supposer que le temps sera réparti également entre une minute et quatre minutes.

Les pièces après contrôle de qualité sont envoyées à la machine M3.

Le temps de traitement dans la machine 3 (M3) est de 10 secondes.

Questionne :

Q1: Calculez le débit moyen par jour de la ligne.

Q2: Calculer l’occupation relative dans le poste d’inspection de la qualité.

Q3: Quelle station est la plus pertinente pour la quantité de sortie de l’usine?

두 번째 라운드에 참가할 준비가 되셨나요?

Plant Simulation학생 챌린지는두 라운드로 Task를 만듭니다 : 전기 모터 최종 조립 작업을 해결하십시오!

지금분기별챌린지에등록하세요!

Plant Simulation챌린지 – 작업 2

Tecnomatix Plant Simulation은 생산 시스템, 물류 및 프로세스의 모델링, 시뮬레이션, 분석, 시각화 및 최적화를 위한 소프트웨어입니다. 공정, 생산 라인 또는 전체 공장의 디지털 트윈을 만들고 새로운 요구 사항에 맞게 개발, 향상 또는 조정할 수 있습니다.

도전의 규칙

Tecnomatix Plant Simulation을 사용하여 주어진 작업을 등록하고 해결하십시오. 여기에서 무료 학생판을 다운로드 하십시오!

수상:

첫 번째 수상자는 Microsoft Surface 터치 스크린 기반 컴퓨터를 받게됩니다! 두 번째 수상자는, 강력한 블루투스 무선 스피커와 세 번째 수상자는, 스마트 시계.

합리적인 솔루션을 갖춘 모든 참가자는 귀하를 Plant Simulation챌린지 참가자로 인정하는 디지털 배지를 받게됩니다.

지금 분기별 챌린지에 등록하세요! →

이 솔루션은 Tecnomatix Plant Simulation을 사용하여 해결해야 합니다.
Siemens Digital Industries Software 및 비즈니스 파트너 외부의 누구나 참여할 수 있습니다.
중요 날짜
과제 발표 : 2022 년 7 월 11 일

제출 마감일 : 2022 년 9 월 30 일

¿Listo para la segunda ronda?

Plant Simulation Student Challenge empieza la segunda ronda: ¡Resuelve nuestro ejercicio de ensamblaje final de motor eléctrico!

¡Regístrese para los desafíos trimestrales ahora!

Plant Simulation Student Challenge – Tarea 2

Tecnomatix Plant Simulation es el software para modelar, simular, analizar, visualizar y optimizar sistemas de producción, logística y procesos. Puede crear un gemelo digital de un proceso, una línea de producción o incluso una fábrica completa y desarrollarlo, mejorarlo o ajustarlo a los nuevos requisitos.

Reglas del Desafío

Registrese y resuelva nuestras tareas dadas utilizando Tecnomatix Plant Simulation. ¡Descargue su copia gratuita para estudiantes aquí!

Premios:

¡El ganador recibirá una computadora basada en pantalla táctil Microsoft Surface! El participante que finalice en segundo lugar, un potente altavoz inalámbrico Bluetooth y en tercer lugar, un reloj inteligente.

Todos los participantes con soluciones razonables recibirán una insignia digital que lo reconocerá como participante del Desafío de Simulación de Plantas.

¡Regístrese para los desafíos trimestrales ahora! →

La solución debe resolverse utilizando Tecnomatix Plant Simulation.
Cualquier persona ajena a Siemens Digital Industries Software y sus socios comerciales puede participar.
Fechas importantes
Anuncio de la tarea: 11 de julio de 2022
Fecha límite de presentación: 30 de septiembre2022

Japanese

ラウンド2の準備はできましたか?

プラントシミュレーション学生チャレンジのタルトをラウンド2に:私たちの 電気モーターの最終組み立て タスクを解決します!

四半期ごとのチャレンジに今すぐ登録しましょう!

プラントシミュレーションの課題 – タスク2

Tecnomatixプラントシミュレーションは、生産システム、物流、プロセスのモデリング、シミュレーション、分析、視覚化、最適化のためのソフトウェアです。プロセス、生産ライン、さらには工場全体のデジタルツインを作成し、新しい要件に合わせて開発、強化、または調整することができます。

チャレンジのルール

Tecnomatixプラントシミュレーションを使用して、与えられたタスクを登録して解決します。今すぐあなたの無料の学生のコピーをダウンロードし てください 詳細はこちら!

賞:

1位の勝者は、Microsoft Surfaceタッチスクリーンベースのコンピュータを受け取ります!2位は強力なBluetoothワイヤレススピーカー、3位はスマートウォッチです。

合理的なソリューションを持つすべての参加者には、プラントシミュレーションチャレンジの参加者としてあなたを認めるデジタルバッジが贈られます。

四半期ごとのチャレンジに今すぐ登録しましょう!→

このソリューションは、Tecnomatix Plant Simulationを使用して解決する必要があります。
シーメンス・デジタル・インダストリーズ・ソフトウェアおよびそのビジネス・パートナー以外の方もご参加いただけます。
重要な日付
タスクの発表:2022年7月11日
提出期限:2022年9月30日

 
 
Matthias Heinicke

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/tecnomatix/logistic-planning-in-universities-material-flow-simulation-for-students/