Products

Solid Edge Tips and Tricks from Forum Users #32

Tips and Tricks from Forum Users #32

An assortment of short tips and tricks based on the discussions in the Solid Edge forum

Compiled by Tushar Suradkar

Due credit is given to respective contributors.

A quick list of the previous compilations:


T&T #01T&T #02T&T #03T&T #04T&T #05

T&T #06T&T #07T&T #08T&T #09T&T #10

T&T #11T&T #12T&T #13T&T #14T&T #15

T&T #16T&T #17T&T #18T&T #19T&T #20

T&T #21, T&T #22T&T #23T&T #24T&T #25

T&T #26, T&T #27, T&T #28, T&T #29, T&T #30

T&T #31

1. Where are the “saved settings” shown in the dialog? How are they created and managed?

Tip: They are created in the Drawing View Wizard (“Saved Settings” button on command bar). It appears they are stored in a “DraftWizard.txt” file located in your “Reports” folder specified in the File Location settings.

Contributor: @KennyG

2. How can I activate the input fields X and Y in the Move command bar?

 Tip: Turn OFF Snap to Grid.

Contributor: @bshand

3. I am getting this error after importing a step assembly and trying to delete items.

Tip: Are you trying to delete a sub-occurrence from a top-level assembly?

I’d suggest to first open the parent sub-assembly of the part you want to delete and then delete the part from there.

Contributor: @TusharSuradkar

4. Someone has broken our template for assemblies, and I need to fix it, making it set to use a BOM setting already created. How in the world do I do this? I opened the template, put an assembly and correct BOM format on the sheet, saved it, then deleted the assembly and the BOM, and saved again. It still reverts back to a bad BOM format. I know I must be missing something simple, but at this point, I can’t find it.

Tip: Go to Solid Edge Options – Drawing View Wizard – Parts List Saved Settings.

Contributor: @Milro

5. I have an assembly and I would like to create a feature on a part in that assembly. I don’t want to create an assembly feature!  How do I edit that part and grab edges and circles from other assembly parts to create the features? I don’t want those features to be dependent on the other assembly components at all. SO when I open that edited part is has a feature that is NOT dependent on the edges, circles, etc. that were pulled from the other components.

Thanks for any guidance​

Tip: Presumably you have “PEERS” enabled……it is located on the Tools tab, while in sketch mode.

Contributor: @SeanCresswell

Tips Compiled by Tushar Suradkar

24_thumb2_thumb_thumb_thumb_thumb_th

Join the Solid Edge User Group on Facebook

Tushar Suradkar

Solid Edge blogger, Programmer

More from this author

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/solidedge/solid-edge-tips-and-tricks-from-forum-users-32/