Hydrogen-powered gas turbines are key to a low-carbon energy future
Discover how B&B-AGEMA are using CFD to design combustors, optimize monitoring equipment, and gain understanding into hydrogen-powered gas turbines.
Energy generation is changing
The world is transitioning to a clean energy future, based on renewable resources such as wind, solar, and hydro. As it makes this change, we still depend on the flexibility of gas turbines for much of our power needs. Turbine-generated power provides the buffer between “base-load” (mainly from coal or nuclear), and inherently intermittent renewable power. Put simply, gas turbines are what keeps the lights on when the sun isn’t shining and the wind isn’t blowing.
The vast majority of the world’s power-generating gas turbines are fueled by natural gas, which is principally the hydrocarbon methane. The industry has worked hard to minimize the harmful emissions from gas turbines. Modern turbines generate 50 to 60% less CO2 per MWh of electricity than a brand new coal-fired power station. However, if we are to avoid a climate emergency, “lower carbon” will not be good enough: we need to turn to zero-carbon energy sources.
The good news is that there is no inherent reason why gas turbines have to burn fossil fuel hydrocarbons. Gas turbines are naturally “fuel flexible”, so attention is increasingly turning towards so-called synthetic fuels such as hydrogen (H) and ammonia (NH3). These fuels contain no carbon, and therefore do not emit any CO2 during the combustion process.
Why move to hydrogen?
Hydrogen is about three times as energy-dense than natural gas (principally methane) and more than twice as energy-dense as gasoline. Better still, burning hydrogen is much cleaner than burning hydrocarbons. When mixed with pure oxygen it only produces water as a by-product of combustion.
Although hydrogen is the most abundant element in the universe, producing, storing, and transporting it on an industrial scale has so far proved challenging. However, Japan is leading the way by committing to an ambitious new plan to become a hydrogen-powered society, starting with the 2021 Tokyo Olympic games, which intends to make a low-carbon hydrogen economy profitable by 2030.
Simulation is key to success
Producing the next generation of low-carbon, hydrogen-powered gas turbines is not without its challenges. It will only be possible through the extensive use of engineering simulation, which can help to optimize the performance, robustness and emissions signature of this new fuel-flexible fleet.
B&B-AGEMA have extensively used CFD simulation to increase the understanding of hydrogen-powered gas turbines, gaining insight into flame shapes and temperatures, mixing, and emission control. They present their findings in detail in this exclusive on-demand webinar. Discover how industry-leading specialists are using CFD to design combustors, optimize monitoring equipment, and gain understanding into hydrogen combustion, including:
- Details on the combustion and turbulence models used in Simcenter STAR-CCM+
- Insights on how B&B-AGEMA used simulation to develop a robust and reliable burner test rig
- How CFD was used in the research and development of the world’s first 100% hydrogen DLN combustor
Register here to watch this on-demand webinar: