Siemens Digital Industries Software Blog Network

Siemens Digital Industries Software Blogs

Thought Leadership

Open energy platforms make sustainable power tech possible – Transcript

As many green energy systems are variable it is difficult to manually optimize them without open energy platforms.
Simcenter

Simcenter Testlab 2606: Faster and smarter next-generation testing, earlier trusted outcomes

Simcenter Testlab 2606 helps engineering teams move faster from measurement to trusted outcomes through a set of next-generation workflows that improve efficiency, confidence, and automation across the testing process. The release enables AI-ready data creation with better context, validation, processing, and workflow automation, expands virtual validation capabilities to support earlier decision-making, introduces free acquisition software for Simcenter SCADAS hardware, and industrializes ISO-compliant blocked force characterization for scalable system-level NVH prediction. Together, these innovations help organizations reduce manual effort, accelerate validation, and make better engineering decisions earlier in development.
PLM Components

What’s New in D-Cubed 2D DCM and PGM Version 80.0

The new release of D-Cubed 2D DCM and PGM v80.0  is now available, delivering new capabilities that help software developers...
Simcenter

Industrializing component characterization for virtual NVH development: Automated component model extraction (AutoCMX)

Simcenter Testlab 2606 introduces Automated Component Model Extraction (AutoCMX), an integrated hardware and software solution that automatically extracts ISO 20270-compliant component models for virtual NVH development. By automating blocked-force characterization and model generation, AutoCMX transforms component characterization from a slow, expert-driven process into a fast, repeatable workflow that produces virtual-prototype-ready models in minutes rather than days.
Simcenter

Virtual shaker testing: Learn before, not during qualification

Qualification testing often happens when risk, cost, and schedule pressure are at their highest. Virtual Shaker Testing in Simcenter Testlab 2606 helps engineers learn before qualification rather than during qualification by creating a real-time virtual representation of the complete test setup. Engineers can predict system behavior, evaluate control settings, validate limiting and notching strategies, and compare virtual and physical models before exposing valuable hardware to full test levels. The result is earlier insight, lower qualification risk, and greater confidence when critical physical testing begins
Teamcenter

PLM reviews rank Teamcenter the #1 PLM software on G2

G2 named Teamcenter Best PLM software for companies of any size - based on customer reviews. Take a look at the PLM software comparison grid to see the top ranking for Teamcenter.
eXplore tour

Siemens eXplore tour brings the future of manufacturing to Rhode Island

At Walco’s Providence facility, local manufacturers and community leaders saw how digital tools can support design, production and maintenance. In...
Simcenter

Stop compromising your test procedure. Schedule it. Re-Runs: None. SCADAS: Agnostic

Simcenter Testlab 2606 introduces Schedule Acquisition for the entire SCADAS family, bringing expert-defined measurement procedures directly into the acquisition workflow. Engineers can now design, automate, and execute complete test campaigns in Simcenter Testlab Neo, ensuring consistent test execution, standardized annotation, and repeatable results across operators, sites, and measurement campaigns.
Simcenter

Achieve greater efficiency in structural dynamics testing with complete next-generation workflows

Simcenter Testlab Neo 2606 introduces complete next-generation structural dynamics workflows that connect virtual instrumentation, data acquisition, modal analysis, virtual point transformation, and model validation in a single integrated environment. New capabilities help engineers streamline setup, accelerate FRF acquisition, improve modal model validation, gain deeper insight into interface dynamics, and strengthen test-simulation correlation, delivering up to 35% average efficiency gains across the structural dynamics workflow.
View our podcasts