Siemens Digital Industries Software Blog Network

Siemens Digital Industries Software Blogs

Simcenter

Sea Fever, an ode to Simcenter Amesim variable sea conditions

Simcenter Amesim 2020.1 includes a variable sea conditions model to consider dynamic impact of waves, wind and water properties on hull resistance.
Expert Insights

Article Roundup: How MaxLinear got faster signoff DRC while optimizing reliability and manufacturability, HLS Powers AI Revolution, Earlier is Better in Latch-Up Detection, Embedding Software Algorithms in New Chip Applications Calls for New Verification, Improving Circuit Reliability

How MaxLinear got faster signoff DRC while optimizing reliability and manufacturability HLS Powers AI Revolution Earlier Is Better In Latch-Up...
Designcenter

2020 Edison Award Winner | Industrializing Additive Manufacturing with HP Inc.

Siemens and HP use CFD-driven optimization to design a revolutionary cooling duct 75% faster than the traditional process.
Simcenter

Bearing Transmission Failures: How to Avoid Them With Virtual Prototyping

Bearings allow complex machinery to rotate by making the rotation possible while reducing friction, and are therefore vital to system efficiency and reliability. Improving bearing design through virtual prototyping is a cost-effective and thorough design approach, which reduces transmission downtime and failures.
Opcenter

AVAILABLE NOW! Opcenter Quality 11.2

We are excited to announce the availability of Opcenter Quality 11.2! Enabling organizations to safeguard compliance, optimize quality, reduce defect...
Embedded Software

What cost cleanliness?

As an engineer/scientist [at heart], I like things that are measurable. Being able to measure something helps me to make...
Partners

Bridging the gap between injection molding simulation and mechanical simulation

We’re going deep fast. How does one simulate the mapping of anisotropic part properties like fiber orientation in injected-molded short-fiber-reinforced...
Simcenter

Keeping it real with Hybrid Multiphase

Around the turn of the Millennium, I was tempted to move away from Engineering, and took a postgraduate course in...
Simcenter

Using water cooling in electronics thermal management - a PC cooling example

Water Cooling? Sounds intriguing, but can liquid cooling be an effective method for thermal management of a PC system? Short...