detectives investigate DFM within a PCB design

The Mysterious Case of the Missing Bowties Part III

Previously… People often say ‘better late than never’, but I’ve never heard my boss say that. After much difficulty in…

The Mysterious Case of the Missing Bowties Part II

Previously… After receiving our boards and having them pass inspection I breathed a sigh of relief as this project was…

The Mysterious Case of the Missing Bowties Part I

It was just another Monday at the office. I had released a design I had been working on for four…

PCB DFM Constraints with Valor NPI

Advanced DFM Constraints management in ADM (Analysis Definition Manager)- Valor NPI 2211

The Analysis Definition Manager (ADM), introduced in Valor NPI 10.0, is a constraints management tool for creating and maintaining sets of Design for Manufacturing DFM rules to be used during the analysis in Valor NPI.

image of an icon representing rigid-flex design

Meeting rigid-flex pcb design challenges with Xpedition

Apart from the typical challenges of PCB design, flex and rigid-flex PCB designers encounter a whole set of unique obstacles….

PCB assembly machine

What is the PCB Design Process?

The PCB design process can be different depending on your company, but the fundamental aspects are all the same –…

PCB manufacturing capabilities

Why is Design for Manufacturing important?

Who is PCB DFM for? For those of us that have climbed a mountain to take in the gaze of…

What's new with Valor NPI DFM software release 11.5

What’s new in Valor NPI v11.5

Valor NPI 11.5 continues to introduce new and existing capabilities in MRA-Revolution, with a more complete Classification set which includes design preparations and analysis use of copper reference layers. Comparing an ODB++ to fabricator changes becomes easy and precise with the new CAM Compare flow and the first connection to stackup setup is established with Z-Planner integration.

IC PCB DFT image

Proactive Design for Test (DFT) best practices

The process of PCB DFT needs to be considered sooner and more proactively in our PCB design process, incorporated in the schematic phase, not during the layout phase. A designer should determine what nets will be needed to be tested based on their likelihood of failure and position those pins in open, accessible real-estate.