Eliminating the silent killer of analog reliability: A structural approach to floating nets
By Bhanu Pandey, Product Engineer, Calibre Design Solutions
A successful first silicon run starts with getting the design details right. Yet, despite increasingly sophisticated design tools, that goal is becoming harder to reach. Recent industry data suggests that first-silicon success for complex analog and mixed-signal designs has hit a historic low of just 14%. While many failures are attributed to parametric shifts or complex noise issues, a significant number are caused by something far more fundamental and harder to detect: the silent killer known as the floating net.
Floating nets in analog power-down circuits represent a hidden reliability risk that can evade even the most rigorous conventional verification flows. As we push for lower power consumption and higher integration, the complexity of power-management schemes grows, and with it, the risk of leaving internal nodes disconnected during specific operating modes.
The hidden risk of power-down circuits
Modern ICs rely heavily on power-down modes to extend battery life and manage thermal profiles. In these modes, MOSFET switches are used to cut off bias currents and isolate entire blocks of the circuit. While this is effective for saving power, it creates a dangerous topological condition. When a block is disabled, internal nodes that were once driven to a defined voltage can lose their connection to any DC path. These nodes become floating.
A floating net is essentially an island in the circuit graph. Without a defined voltage, its potential is determined entirely by leakage currents and capacitive coupling. Over time, these nodes drift unpredictably. This drift is not just a theoretical concern; it has real-world consequences:
- Unintended transistor activation: A floating gate can drift to a voltage that partially or fully turns on a transistor that should be off.
- Unregulated power routing: If a pass transistor in a regulator is accidentally activated, it can route unregulated power to sensitive downstream components.
- Device damage: Unpredictable voltages can lead to overstress conditions, causing permanent damage to thin gate oxides or other sensitive structures.
- Silent failures: These issues often don’t show up in standard functional tests but manifest as intermittent reliability failures in the field, leading to expensive recalls and brand damage.
Why conventional spice simulation fails
If floating nets are so dangerous, why doesn’t standard SPICE simulation catch them? The answer lies in the difference between parametric behavior and topological structure.
Conventional simulation is designed to model the behavior of a circuit based on a set of parameters and a specific testbench. It faithfully simulates exactly what was designed. If a designer forgets a pull-up resistor or a DC path, the simulator will model the circuit without it.
The blind spot exists because a floating net is a structural defect – a missing connection – rather than a parametric failure. To catch a floating net via simulation, a designer would need to:
- Know exactly which node might float.
- Create a testbench that exercises the specific power-down configuration where the float occurs.
- Simulate for a long enough duration to allow leakage currents to cause a visible drift.
In a design with thousands of nodes and hundreds of power-down states, the number of permutations is astronomical. It is virtually impossible to cover every scenario with simulation alone. Consequently, these defects often remain hidden until the first silicon returns from the fab.
Introducing structural signoff with Insight Analyzer
To close this gap, designers are turning to a new methodology: structural signoff. Instead of trying to simulate every possible behavior, structural signoff analyzes the underlying circuit graph to identify topological defects that guarantee unreliable behavior, regardless of parameters.
Siemens’ Insight Analyzer is at the forefront of this shift. It analyzes the circuit’s structure rather than its behavior. By starting from known voltage sources (like VDD and GND) and propagating them through the circuit graph, it can instantly flag any net that lacks a DC path to a defined voltage under any given enable/disable configuration.
Key benefits of structural analysis
- No testbench required: Because it analyzes the topology, it doesn’t need a complex simulation environment or stimulus.
- Comprehensive coverage: It examines every net under every possible power state, covering scenarios that simulation would likely miss.
- Pre-layout detection: Insight Analyzer can run on pre-layout schematics, allowing designers to find and fix Priority 1 defects before they ever reach the layout stage.
- Speed: Analysis that would take days or weeks of simulation time can be completed in seconds or minutes.
Case study: the LDO victim net
To illustrate the power of structural signoff, let’s look at a common CMOS Low Dropout (LDO) voltage regulator. This LDO features a standard enable/disable function designed to save power when the regulator is not in use.

In this design, an error amplifier (OA1) drives the gate of a PMOS pass transistor (Mp_pass). The connection between the amplifier output and the pass transistor gate is a critical node, which we’ve labeled the VICTIM net.
When the enable signal (EN) is high, the LDO operates normally. However, when EN goes low to power down the circuit, the MOSFET switches within the error amplifier cut off the bias currents.

As shown in the power-down state, the VICTIM net is suddenly isolated. It no longer has a DC path to a defined voltage. It is now floating. In this state, leakage currents could cause the gate of the pass transistor to drift low, accidentally turning on the regulator and sending unregulated voltage to the output.
Using conventional SPICE simulation, this defect might never be noticed unless the designer specifically looked for drift on that gate during a long power-down simulation. However, Insight Analyzer identified the issue almost instantly.

The tool flagged a Priority 1 “Float, conditional” violation. It proved that the net enters a high-impedance state (z) whenever the EN node is driven low. The analysis was completed in seconds, providing the designer with a clear, proven violation to address.
The fix: Minutes vs. millions
Once a floating net is identified, the fix is usually trivial. In the case of our LDO, the solution was simply adding a small PMOS pull-up transistor to the VICTIM net, gated by the inverse of the enable signal. This ensures that whenever the circuit is disabled, the VICTIM net is actively driven to VDD, keeping the pass transistor safely turned off.
This fix took only a few minutes of design work. Compare that to the alternative: discovering the defect in the lab after the first silicon arrives. A respin to fix a single missing pull-up can cost months of delay and millions of dollars in mask costs and lost market opportunity.
Conclusion: shifting left for reliability
The 14% first-silicon success rate is a wake-up call for the industry. We can no longer rely solely on simulation to catch every defect in increasingly complex analog designs. By shifting left and incorporating structural signoff into the verification flow, design teams can eliminate the silent killers like floating nets early in the cycle.
Insight Analyzer provides the structural insight needed to ensure that analog circuits are not just parametrically correct, but topologically robust. In a world where a single missing connection can lead to a multi-million dollar failure, structural signoff isn’t just a luxury – it’s a necessity for modern IC reliability.
Learn more in our new whitepaper Finding floating nets in analog circuits with Insight Analyzer