DRC at scale: How Calibre Vision AI turns billions of errors into actionable insights
Facing the mountain of DRC errors at advanced nodes
If you design advanced SoCs, you know that DRC runs at leading-edge nodes (2 nm, 3 nm and below) can be brutal . It’s not unusual for a full-chip check to turn up hundreds of millions—or even billions—of violations right out of the gate.
Instead of simply checking a box and moving forward, design and verification teams are hit with an avalanche of errors that must be sorted, sifted and fixed. Navigating this mountain of data with traditional tools is an exercise in frustration, one that slows tapeout and threatens project schedules.
But with growing design density and restrictive process rules, this challenge is now the norm for advanced node SoC projects. “Dirty” initial result sets appear precisely when block interfaces, power intent and layout constraints are still evolving. Standard batch-oriented debug workflows delay much-needed visibility until long after the check is complete, forcing teams into long, serialized cycles of checking, then fixing, then rechecking. The opportunity for improvement is clear and that’s where Calibre Vision AI can make a transformative difference. It takes billions of DRC violations and turns them into a shortlist of real, actionable issues, so teams can get to work faster (figure 1).

From batch bottleneck to continuous, real-time insight
Classic DRC debug is a batch-oriented, sequential process. You generate a full-chip DRC run and then wait—sometimes for hours or even days—before analysis can even begin. Each hour spent waiting is time that could otherwise be used for debugging, tracing root causes or moving the project toward signoff. This traditional flow feels particularly outdated in the context of massive, modern SoC designs (figure 2).

Calibre Vision AI changes the game by transforming DRC debug into a continuous, parallel and collaborative activity. Instead of waiting for the entire DRC run to finish, you can now start analyzing, prioritizing and debugging even while checks are still in progress. This “shift left” approach keeps everyone productive, enables real-time decision-making and helps designs converge faster—even as data volumes skyrocket.
Real-time incremental results loading
One of Calibre Vision AI’s breakthrough capabilities is incremental OASIS results database loading. Instead of being forced to wait for all results to generate and post-process, designers can launch the tool as soon as the Calibre nmDRC job starts and results will begin streaming into the environment live. This means every new violation is available for review as soon as it’s found. Because the OASIS result database is a fraction of the size of a comparable ASCII result file, incremental loading is both fast and lightweight (figure 3).

This approach pays dividends: DRC checking and debug can occur in parallel, so catastrophic or systemic issues are caught early and teams can often fix constraints or integration glitches on the fly—no need to lose an entire DRC iteration to one bottleneck. This is a fundamental productivity boost that wasn’t possible with traditional tools.
Instance-complete results: No more hidden DRC errors
One of the biggest sticking points in classic DRC workflows is incomplete visibility. Older DRC tools commonly limit the number of errors reported per check which mask a significant systemic issue from being discovered in the current iteration. The result? Significant issues get buried, requiring multiple DRC iterations and repeated cycles just to see the full picture.
Calibre Vision AI addresses this directly via its instance-complete results technology. By capturing every violation across the entire hierarchy and all block instances, it ensures nothing gets hidden by arbitrary reporting limits. With OASIS as the data backbone, designers get complete, across-the-die visibility in a single run. No more guesswork or endless loops chasing elusive errors. This comprehensive approach is essential for reliable and predictable DRC convergence, reducing wasted debug cycles and helping teams move confidently toward closure (figure 4).

For example, if a deeply nested SRAM macro triggers a violation in a routing constraint, that error is captured and exposed—the team doesn’t need to wait for later iterations to discover additional issues in “hidden” logic. This transparency empowers teams to address design problems holistically in the first iteration, dramatically compressing debug time.
AI-guided signal grouping: From billions of violations to actionable insights
Sorting through a billion raw DRC results feels like finding a single needle in a haystack made entirely of needles. With so many violations, distinguishing noise from actionable issues is often left to “best guess” prioritization, manual scripts and endless error tables.
Calibre Vision AI introduces AI-guided Signal grouping to cut through the chaos. Here’s how it works: Individual DRC violations are analyzed for spatial and semantic similarities, then clustered into “Signals,” each representing a unique failure pattern or debug entry point. Instead of dumping endless lists, Calibre Vision AI reduces billions of violations to a few hundred Signals—each an actionable target for engineering teams (figure 5).

To take focus even further, Signals are distilled into “Signatures.” These capture recurring failure behaviors across the die, pointing to systemic design or integration problems. With grouping at the core, teams move from analysis paralysis to intelligent triage—tackling the highest-value problems first, tracing root causes efficiently and making measurable progress on every DRC iteration.
A practical scenario: Early in a design cycle, a team discovers that billions of errors are related to just a handful of “signature” cell boundary conditions. Instead of spreading effort thinly across thousands of unrelated violations, engineers can focus on fixing a small set of layout constraints—dramatically improving closure speed and design quality.
Real-world productivity: Parallel debug, faster convergence
Traditional DRC workflows require that the debug process begins only after all DRC violations are written out and checked. This creates serial bottlenecks—no work can start until the last result is written and processed, delaying both root-cause analysis and closure.
Calibre Vision AI introduces a parallel debug approach: Chip-level DRC checking and debug work can proceed side-by-side, with results incrementally loaded into the user interface. Chip owners can collaborate with partition owners in real time, triaging errors and handing off fixes as problems are found—not hours later. The result? Drastically reduced DRC iteration times and much tighter coordination across the entire project team.
Global filtering and focused navigation
Navigating billions of DRC violations can overwhelm even the most experienced verification teams. Calibre Vision AI addresses this challenge with Global Check Filters and Global Cell Filters to sharpen focus on relevant errors (figure 6).

Combination filters using Boolean options enable highly customized result views. Applied filters persist across sessions and dynamically update all panels for seamless, context-aware navigation.
Review, handoff and traceability
Calibre Vision AI enhances collaboration by allowing workspace layouts—including filter settings, debug context and selected Signals—to be saved and handed off.
Export capabilities make reviewing, sharing and handing off debug results fast, simple and traceable (figure7). Results are context-aware, supporting both chip-level and block-level debugging. This ensures that team members can pick up right where the previous work left off.

Exporting results in chip-level context is invaluable for SoC integration teams, while partition owners can receive block-specific exports for efficient problem-solving.
Calibre Vision AI: A smarter way to drive DRC closure
Ultimately, Calibre Vision AI is more than a productivity tool—it’s a platform for transforming the way teams approach physical verification at scale. Instance-complete results eliminate guesswork, AI-driven grouping helps prioritize what matters and real-time incremental loading turns traditional bottlenecks into opportunities for early action. Advanced filtering and workspace handoff further enable collaboration and traceability.
For SoC physical verification engineers, debug specialists, design team leads and EDA tool methodologists working at advanced nodes, these capabilities help unlock reliable, predictable DRC convergence in a world where the error count feels unmanageable.
The benefits are clear:
- Catch and prioritize issues early, triage them efficiently and maintain focus on real closure.
- Shorten DRC iteration cycles for quicker, more reliable signoff.
- Boost team productivity and improve overall design quality—by cutting time waste and reducing the risk of project surprises.
Bonus content! We also have a technical paper on this very topic that takes an even deeper dive into the details. Access the paper here: From billions of violations to actionable insights: Calibre Vision AI | Siemens
Want to hear more about how teams can navigate the mountain of advanced node DRC? Check back soon for Part 2 of this series that will explore how collaborative debug workflows, advanced filtering, persistent workflow tracking and seamless handoff are further changing the game.