What STEP was for CAD, ECXML is for electronics thermal simulation

‘Electronics Cooling eXtensible Markup Language’ (ECXML) is a neutral file format intended to facilitate the provision of thermal models from suppliers to end users, for use in 3D CFD thermal simulation tools such as Simcenter Flotherm, Simcenter Flotherm XT and Simcenter FLOEFD. A defacto standard for a number of years, ECXML is now published by JEDEC as the JEP181 guideline.

A brief history of electronics thermal standardisation

Best practices and proprietary data formats can be developed by any provider of software tools used to ensure thermal compliance of electronic products (or any product that contains electronics). However, to ensure mass adoption by the industry, standards bodies play a key role.

The JEDEC JC15 committee focuses on writing thermal standards to create a common reference point for the generation of thermal characterization data and thermal models. Siemens involvement with JC15 goes back to the mid ’90s where, as Flomerics, having led the EU funded ‘DELPHI’ project, we sponsored the standardisation of a method to extract BCI (boundary condition independent) CTMs (compact thermal models) of IC packages, published as JESD15-4. In addition JESD15-3 was published covering the simpler, but more common, ‘2-R’ CTM.

Supporting the thermal model supply chain

There are a range of electronic thermal simulation tools available on the market. There is also a requirement that a supplier of parts or sub-assemblies provide thermal models of their products to be simulated in their customer’s operating environments. Forcing a supplier to provide multiple proprietary formats that support these multiple tools is an onerous undertaking and one that, to date, has limited the availability of such simulation models.

Just as the IGES format published in 1980 and the STEP format published in 1994 (for representing 3D CAD data) helped revolutionise the adoption of CAD tools, there has been no analogous format for electronic thermal models, until now.

ECXML open file format

Proposed initially by Mentor – A Siemens Business, this XML Schema can represent thermal modelling objects that are common between a range of commercially available electronics thermal simulation tools. Round Robin testing with other simulation tool vendors confirmed the format in 2015.

Both import and export of ECXML was then supported in Simcenter Flotherm.

Simcenter Flotherm ECXML Import Dialog box (JEDEC JEP181 support)
Simcenter Flotherm ECXML file format import

Now that suppliers had the ability to generate and provide a single neutral format that could be imported into a number of downstream simulation tools, as opposed to supplying multiple proprietary formats, many of the barriers to model supply that existed previously were removed.

ECXML now published as JEDEC JEP181

In 2019 a JEDEC JC15 ECXML working group was set up, with representatives from all major thermal simulation software providers and key electronics companies, which I had the honour of chairing. The intention was to standardise what had already become an industry defacto ECXML standard.

To do so a Guideline document was created, as an adjunct to the ECXML Schema, describing the format, the importing software specific interpretation of the ECXML data and a demonstrative worked example:

ECXML file format guideline exerpt from JEDEC JEP181 (Simcenter Flotherm workflow illustrated 1)

Unanimously passing both JC15 Committee and JEDEC Board of Directors ballots, the Guideline and associated ECXML schema were published as JEP181 on 17th September 2020.

Overcoming data availability limits in electronics thermal analysis

As a thermal engineer tasked with predicting operating junction temperatures of a proposed design in a specific operating environment, the main issue you might face is lack of available data necessary to construct your thermal digital twin.

The standardised availability of ECXML will make available the data that you require, reducing time wasted on hunting down the information you need to perform your tasks, increasing your productivity and ability to innovate!

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/ecxml-jedec-jep181-thermal/