Products

How end-of-line testing can automate product fault detection

In the automotive sector, end-of-line testing uses vibroacoustic measurements to automatically and objectively detect faulty parts in the production line. Learn how automated measurements can help you minimize quality issues. And understand also how to optimize this process.

Every product undergoes some form of testing at the end of the manufacturing process, but some tests are better than others. Do you have the capability and functionality to carry out the most extensive EOL testing without blowing your budget?

A century-old technique

In fact, vibroacoustic measurement has been a trusted end-of-line testing method to detect faults and defects in manufacturing since antiquity. Indeed, when a ceramist just finishes producing a series of fine pottery vases, how can he detect potential invisible flaws in the structure of the delicately crafted objects? He might gently tap every single vase. And he listens carefully to the acoustic response. Does the structure sound healthy and whole? Or does it produce a dull tone, hinting at the presence of small air bubbles or tiny cracks under the flawless surface?

Indeed, from the ancient ages through the Industrial Revolution to the modern digital age, noise and vibration measurements have helped reveal many defects. In modern times, vibroacoustic measurements using calibrated sensors have become an automated, objective method to test high volumes of mass-produced parts. But how do you apply and implement automated testing the right way?

Close-up view of a ceramist making a pottery vase
Ceramist handcrafting a vase.

Why end-of-line testing is important

Just like our handcrafted vase, noise and vibration testing can assess the quality of many parts and manufactured products. Yet, many companies are still not aware of this opportunity. Some consider a product’s vibration behavior a secondary characteristic. They focus their attention on other, more tangible product attributes such as its design, surface quality, or color. But what lies beneath the shiny surface of the item is just as important as its appearance.

Indeed, a product’s true quality is revealed only during operation. Does it function flawlessly according to expectations, or does it vibrate abnormally? Excessive noise and vibrations are often a sign of a production defect that has gone unnoticed so far. From the imperfections in the finish of a gear tooth to the imbalances of a bearing part, you can hear and feel the defects, even without seeing them.

How can noise and vibration testing be used to your advantage and reveal defaults in the parts early in the manufacturing process?

Automated vibroacoustic measurements offer a fool-proof method to rapidly test every single part that comes off the production line for its quality.

A man works on an engine in the production line
A man works on an engine in the production line

What should you test? 

In fact, every moving part and piece of a mechanical machine can, and should, be tested for its vibro-acoustic behavior. This includes:

  • Parts of and whole internal combustion engines, of all sizes and for all applications
  • Parts of and whole electric motors, of all sizes and for all applications, from the powerful traction motors down to the tiny windscreen wiper motor or the seat adjustment motor
  • The extremely fast turning parts of turbochargers
  • All types of compressors for air-conditioning units or for refrigerators

The applications of systematic end-of-line testing are not limited to parts produced for the automotive industry. Other industries can also benefit from the trusted method.

Even single components and non-moving parts are suitable test subjects. The method called acoustic resonance testing consists in exciting the part, for example, by hitting it with a small impact device and listening to its acoustic and vibration response. This method helps identify imperfections like cracks, cavities, improper heat treatment, wrong or missing material, and many more. Check out this blog post for the end-of-line testing definition for electrified powertrains.

How to implement vibroacoustic end-of-line testing

So, now you understand why you should implement end-of-line testing. But how should you do it?

As with many other defect detection methods, it is best to rely on the knowledge and experience of a trusted partner. If you want to meet the demands of industrial quality testing, you should ask him questions such as:

  • Which sensors should I use and where should I position them?
  • How can I catch the signal of interest using highly sophisticated trigger mechanisms?
  • Which analysis functions and evaluation algorithms should I apply?
  • How can I build a test bench?
  • How should I design the test cycle?
View of a car engine production line
Manufacturing car engine parts.

Introducing Simcenter Anovis

Siemens experts can help you with the questions above when you implement the Simcenter Anovis solution. Simcenter Anovis is a robust and reliable industrial quality testing system. It is easy to integrate into end-of-line test benches and production lines. It helps deliver product quality at lower production costs while preventing production line outages and reliably identifying defects.

Beyond simple fault detection, Simcenter Anovis also provides deeper, valuable insights into the product’s characteristics. These insights foster product enhancements or innovations. Indeed, they clearly point at the possible root cause of the identified problem. This information is not only valuable for the manufacturing team, which consequently implements improvements along the production line. It is also useful for the research and development teams, as a reliable, real-life input into future product enhancements.

Simcenter Anovis is a complete system, not a DIY tool kit. Implementing Anovis includes:

  • free technical consulting, explaining the benefits and defining the limits of vibroacoustic defect detection
  • adapting the modular hardware and software according to your tasks and process needs
  • realizing feasibility studies to ensure the applicability of new tasks
  • commissioning at the test bench builder and/or in the production environment, including the initial parameterization of the system’s communication and signal analysis
  • operator training and customer services, tailored to the requirements of industrial production standards
Implementing quality inspection for end-of-line testing equipment is key to avoiding extra costs related to rework, product recall, or the loss of stakeholder and customer trust.

How does Simcenter Anovis work?

Firstly, the Simcenter Anovis system collects data from a wide range of sensors over a large bandwidth. This data includes vibration from accelerometers or laser vibrometers, sound from microphones, rotational speed from high-precision tachometers, temperature, and torque. Of course, all of it is accurately recorded with the Anovis hardware.

Then, the dedicated Simcenter Anovis software for test bench control initiates a smart signal analysis of the data. It performs precise pass/fail checks for each object under test. With the software, users can also analyze the recorded signals, employing smart analysis methods in the frequency, order, angle, and time domains. As a result, they can reliably detect relevant fault patterns.

The system also applies statistical assessment procedures to dynamically tune the testing thresholds. These procedures turn Anovis into a self-learning system that gradually reduces the required setup effort and operation expertise. The responsible team can thus easily deliver a formal quality report that confirms that the part meets the required specifications and operates safely.

Do you want to learn more about this topic?  Read the white paper or join our free on-demand webinar “End-of-line testing for automotive: How to perform NVH-based quality inspection”.

You will learn how to effectively:

  • build a robust and reliable end-of-line testing
  • integrate an efficient end-of-line quality system
  • determine product faults by analyzing the acoustic signature

For more information?

For more info about the Simcenter Anovis functionalities, please read the article: Simcenter Anovis for end-of-line quality testing. Or, check out the technical on-demand webinar series.

Elif Altuntop Kavas
Technical GTM Specialist

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/how-end-of-line-testing-can-automate-product-fault-detection/