Products

Engineering the bowling experience with Simcenter X

Engineers solving complex product challenges today face a critical bottleneck: fragmented simulation toolchains. Running system-level dynamics in one tool, computational fluid dynamics (CFD) in another, and finite element analysis (FEA) in a third creates workflow friction, licensing complexity, and infrastructure constraints that slow innovation.

Simcenter X changes that. As Siemens’ cloud-native engineering platform, Simcenter X brings multi-physics simulation capabilities—system simulation, CFD, structural analysis, and design optimization—into a unified environment with flexible cloud licensing and on-demand compute.

To demonstrate how this works in practice, we built a playful but technically rigorous case study: engineering the perfect bowling strike. While bowling might seem lighthearted, the physics involved—trajectory prediction, aerodynamic analysis, structural impact, and optimization—mirror the same multi-physics challenges engineers face in automotive, aerospace, and industrial machinery design.

Here’s how we used four Simcenter X tools to simulate, analyze, and optimize every aspect of the bowling experience … and what that reveals about modern cloud-native engineering.

A tour through bowling history

Our story begins 5,200 years ago in ancient Egypt! Archaeologist Sir Flinders Petrie found small stone balls and nine miniature pins in a child’s grave. While we can’t say if little Tutankhamun was practicing his spares, it’s definitely early bowling!

Fast forward to Germany around 300 AD, where bowling got spiritual: parishioners rolled stones at a “Kegel” (pin) representing sin. Knocking it over symbolized cleansing—hence “kegling.”

When European settlers brought Nine-Pin Bowling to America, it sparked so much gambling that states banned it in the mid-19th century. The ingenious solution? Add a tenth pin to create “Ten-Pin Bowling,” completely sidestepping the ban!

Finally, the late 19th and early 20th centuries brought rules, standardized ball weights, and dedicated indoor alleys, turning it into the year-round sport we know today.

From ancient rituals to a global sport, bowling has certainly had an incredible journey. And today, this fascinating evolution continues, with Simcenter X enabling engineers to precisely understand, optimize, and simulate everything from the perfect ball trajectory and the complex physics of pin behavior for an even better game. Best of all, it brings all these multi-physics studies together onto a single cloud-native platform – powered by a flexible, single-license model that handles everything from initial concept to final optimization without skipping a frame.

Simulating success: Achieving the perfect digital strike (X) using Simcenter Amesim

Using Simcenter Amesim and its 3D Mechanical Library, we built a system simulation model designed to accurately predict the trajectory of a bowling ball down the lane. The model accounts for all the core physical dynamics—from the initial ball spin, ball lateral offset and launch force to lane friction and pin collisions.

To make these complex physics accessible and fun, we paired the backend model with a custom Python app. The app lets users easily adjust shooting conditions and instantly visualizes the result with an interactive 3D animation.

Now it’s up to you, player—step up to the lane and score the perfect digital strike(X)!

Perfecting the digital strike using Simcenter HEEDS

But can we compute the exact initial conditions needed to trigger our desired perfect score?

Enter Simcenter HEEDS—an intelligent design exploration and optimization software that automatically searches through design variations to find the optimal setup required for a perfect strike (X). Because multiple combinations of these variables can lead to the same winning outcome, Simcenter HEEDS maps out the possibilities effortlessly.

Best of all, with Simcenter X and its flexible cloud licensing, you can seamlessly switch between Simcenter Amesim and Simcenter HEEDS on the fly, unlocking powerful cloud-scale optimization without missing a beat.

Analyzing pin aerodynamics using Simcenter STAR-CCM+

Why stop at the ball? With Simcenter X, we can take things to a whole new aerodynamic level using Simcenter STAR-CCM+. Ever wonder how a bowling pin cuts through the air? Simcenter STAR-CCM+ lets us run high-fidelity Computational Fluid Dynamics (CFD) to analyze pin aerodynamics and wake turbulence. Because let’s be honest—when you’re trying to annihilate ten pins, knowing the drag coefficient of a maplewood pin is vital, highly scientific, and mostly just an excuse to make colorful rainbow gradient animations.

Simulating a bowling pin’s worst nightmare with Simcenter 3D

Sure, sending a high-speed ball down the lane looks fun to us, but have you asked the pins how they feel about it? Using Simcenter 3D (powered by Simcenter Nastran), we subjected our virtual bowling pins to finite element method (FEM) analysis to see what happens during maximum-impact trauma.

Instead of just watching them fly, Simcenter Nastran lets us look deep inside the maplewood to map out stress concentrations, structural deformation, and shockwaves. It turns out that getting smashed by a heavy sphere traveling at high velocity results in extreme structural agony.

Strike (X) on the cloud: Why Simcenter X changes the game

Simcenter X is our cloud-native engineering environment that brings Siemens’ industry-leading simulation tools together into a single, highly flexible ecosystem. Instead of being locked to heavy local hardware or juggling separate licenses, Simcenter X gives you on-demand access to high-performance cloud compute and multi-physics capabilities—from 1D system simulation and CFD to structural FEA and design optimization.

In our world, that means you don’t just simulate a bowling ball rolling down a lane—you can use Simcenter Amesim to simulate a bowling ball rolling down the lane, scale up massive cloud compute to run aerodynamic wake analysis on the pins with Simcenter STAR-CCM+, torture-test them with Simcenter 3D Nastran, and let Simcenter HEEDS hunt for the exact launch spin and force required for a guaranteed strike, all under one seamless cloud license. It removes all the IT friction so you can focus on the physics, whether you’re engineering complex industrial machinery or just trying to achieve digital bowling perfection.

Miguel Cabezas Vega
Simcenter System Simulation Customer Support Manager

System simulation: unlocking potential, solving problems, and making life easier.

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/engineering-the-bowling-experience-with-simcenter-x/