Siemens Digital Industries Software Blog Network

Siemens Digital Industries Software Blogs


Verification Horizons

High-Level Design Validation and Test (HLDVT) 2010

I’ve had the pleasure of participating in the IEEE International High-Level Design Validation and Test (HLDVT) workshop off and on...

Verification Horizons

New OVM Sequence Layering Package – For Easier Tests

Download Now A new OVM Layering Package that provides a means to add layers of tests (sequences) without modifying the...

Simulating the Real World

The art of modelling using CFD. Part I - What happens if you cross art with science?

Considering that CFD (Computational Fluid Dynamics) is an advanced mathematical method for predicting fluid flow and heat transfer using a computational...

Verification Horizons

OVM 2.0 Register Package Released

In January 2010 we released the OVM 1.0 Register Package.  It has now been updated to enhance capabilities and address...

Embedded Software

OS influence on power consumption

Power consumption is an issue. With portable devices this affects battery life. [I am irritated by the short intervals between...

Corporate Blog

Want to Design a Factory?

This is not an easy task as the amount of information to take into account is huge. Starting with architectural information like the plant layout to libraries of standard manufacturing equipment whic...

Embedded Software

iPad impressions

I am not an Apple fan. I do not mean that I have anything against the company. Far from it...

Polarion

Polarion 2010-SR1 now available

Service Release 1 (SR-1) for Polarion 2010 is now available. The release delivers some new features and significant improvements in additions to bug fixes and general improvements: Polarion insta...

Embedded Software

ESC Silicon Valley 2010

As usual, I attended the Embedded Systems Conference in San Jose, CA last week. I guess it remains the foremost...