Article Roundup: Automotive Smart FET Driver ICs, ISO 26262, Most Innovative Product Award, IoT, RTOS Scheduling
August 04, 2017
ON Semiconductor Meets AEC Challenges with Electrothermal Analysis Rob Bates on Safety and ISO26262 Embedded Computing Design announces 2017 Most...
By Expert Insights
2
MIN READ
Simcenter
Showing the LMS SCADAS XS at Automotive Testing Expo
August 04, 2017
These days passengers expect to feel comfortable in their cars. The bar is set high. As a result, there is an increasing need to check Noise, Vibration and Harshness (NVH) during test drives. Enginee...
By ChristopheC
2
MIN READ
Polarion
Confidence in the Use of Software Tools per ISO 26262
August 04, 2017
The preeminence of the ISO 26262 standard, the adaptation of IEC 61508 to functional safety needs specific to road vehicles, is indisputable. Fundamental to ISO 26262 compliance in the ...
By borsem
4
MIN READ
Teamcenter
Digital Disruption Challenges IT to Reach New Efficiency Levels
August 03, 2017
Digital disruption puts IT at the front end of the business. In the business of IT, you can be pretty modest about your achievements, when in fact administering and maintaining a PLM system is ...
By Margaret Furleigh
3
MIN READ
Embedded Software
Communication breakdown
August 03, 2017
I often marvel at the fact that I now live in a science fiction world. At least, a lot of...
By Colin Walls
4
MIN READ
Opcenter
Using Quality Systems to Gain Efficiency – Is that even possible?
August 03, 2017
Cost and Quality. They are often thought of as two sides in a game of “tug of war.” When one side gains traction the other loses. However, that is a very non-strategic view of how well-architected ma...
By
2
MIN READ
Designcenter Solid Edge
3D Sketching: The future of sketching in CAD
August 02, 2017
In mechanical CAD, sketching is the basis for creating 3D models. Now, there are exceptions e.g. using synchronous technology in Solid Edge, you may not need sketching at all if the model is made up ...
By SandeepM
6
MIN READ
Opcenter
Why focusing on Quality rather than Compliance makes good business sense
August 02, 2017
In medical device manufacturing, as well as other regulated industries, we have served two masters. One is the end consumer, without whom we have no business. The other is the FDA (or other regulator...
By Riccardo Consonni
2
MIN READ
MindSphere
MindSphere Release July 2017
August 01, 2017
Hereby the offerings MindAccess User, MindAccess Developer and the new MindConnect Elements MindConnect FB 1500 and Mind Connect LIB are released for sales and delivery. The new MindA...
By dvidflrmnd
6
MIN READ
Posts navigation
«
1
…
1,485
1,486
1,487
1,488
1,489
…
1,972