Thought Leadership

3 more embedded software tips

In my occasional series of tips for embedded software development, I have three more. This time they are all associated with C/C++ programming …

A lot of embedded programming is about paying attention to details, particularly when using the power of the C language, when there is no safety catch. 🙂

Take care to ensure that an array index never goes negative

Arrays in C/C++ start from zero and go up to n-1 where n is the size of the array. This is straightforward, but there are two issues to think about: underflow and overflow. And these do need to be considered as there is no “run time system” to stop you making mistakes. First, overflow. It is not too hard to avoid running off of the end of array, it just needs code like this:

#define N 99
int arr[N];
for (i=0; i<N; i++)
   arr[N] = i;

Just make sure that < is never replaced by <= …

To me, starting counting at zero is totally intuitive, but I started out with assembly language programming, where that is obvious. Just do not let an index get negative. This code is entirely valid:

arr[-5] = 99;

but stupid.

In C, do not set the size of an array that will hold a string; let the compiler do it

When you create an array in C that is going to hold a text string, you have two things to think about. First, you need to be sure that you know how/when the data will be placed into the array. Most embedded development toolkits take care of that, but you should be sure that you know what is going on.

The second point is array size. You could write this:

char str[13] = “Hello world!”;

That would be fine.There are 12 actual characters and a NULL terminator. Alternatively, this is easier:

char str[] = “Hello world!”;

The compiler can count! Interestingly, you can also do this:

char str[12] = “Hello world!”;

which creates a string without a NULL terminator. This would save a byte of memory, if you knew the string length elsewhere. Note that this is illegal in C++.

If a text string is never going to be changed, there is no point in it being in a program section that is [logically] in RAM and this code might be better:

char *str = “Hello world!”;

Never assume the size of data types in C/C++

The traditional data types in C – int, unsigned, char, etc. – are really non-ideal for most embedded applications, when the actual size of data is [or needs to be] know. It is much better to define typedefs with meaningful names – like UINT32 – or use a newer C language variant and utilize the rational data types like uint32_t.

Colin Walls

I have over thirty years experience in the electronics industry, largely dedicated to embedded software. A frequent presenter at conferences and seminars and author of numerous technical articles and two books on embedded software, I am a member of the marketing team of the Mentor Graphics Embedded Systems Division, and am based in the UK. Away from work, I have a wide range of interests including photography and trying to point my two daughters in the right direction in life. Learn more about Colin, including his go-to karaoke song and the best parts of being British: http://go.mentor.com/3_acv

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/embedded-software/2019/11/11/3-more-embedded-software-tips/