Products

AA battery replacement project tutorial #6:  AA Tabs

Continue

This entire project is intended to be done within the free trial period.

[This is Part 6 of the tutorial, for Part 1 click HERE]

Open Schematic

Double click your saved schematic to open and continue where we left off from

New Schematic Sheet

Let’s create a new schematic sheet. Do you remember how to do so?

… Yup! You can just look it up as in the image below:

Reminder Tip:

You can pin the menus you like anywhere,

you can also set shortcuts for them,

OR check which shortcuts already exist.

You can ask the ✨Product Support Copilot✨ how to do any of this.

Another Reminder Tip:

There are two types of shortcuts:

  1. Regular Keyboard shortcuts
  2. Mouse “strokes,” as in just draw any shape with your mouse!

There are already default ones set for you, but you can set your own or change the default ones too!

Design Navigator

Make sure your Design Navigator is open. If it isn’t, you can use the search tool to find it and pin it.

You can also right click on the sheet in the Navigator to rename it (e.g. AA Tabs):

Components

Arrange Components

Arrange your components so that they look something like the image below.

Reminder Tip:

Click CNTRL + R to rotate components

ANOTHER Reminder Tip:

Want to turn off pin number attributes?

Of course, you can ask the Product Support Copilot how to. But here’s a quick way to do it:

  1. Double click the actual PIN itself
  1. When the properties tab opens, simply untick the pin number

Place Power Symbols

Do you remember how to do so?

There are many ways to place a power symbol.

My favourite is always to find anything I want through the search bar as in the following image.

Once you place it, you can right click to select properties, and change its name.

Create:

  1. +3V

Place it as in the following image:

Place Ground

Remember how to do so?

You guessed it, you can just look this one up too!

Now place GND as in the following image:

Place Net

Reminder Tip:

Click n (lower case) to place a net

So go do your thing and place nets to connect components as in the following image:

Scale Components Symbols (grow/shrink)

You might want to make your 0R links smaller than the rest of the components. If so, the steps are:

  1. Click the component you want to scale to a different size (I did this for all the 0R)
  1. In the search tool, look up “scale”
  1. Choose the scale factor you like

Place Text (Reminder)

Can you guess how to place text?

Yup, look it up through the search bar and you can find it in an instant!

Now, can you guess how to edit it?

If you guessed right click → properties, then you’re absolutely correct!

Place text as in the image below, or wherever you see fit.

 

Reference Designators

We will do this at the very end, so worry about this for now!

That’s it for today!

Save and close your project, and let’s continue next time. Let me know if you enjoyed this tutorial in the comments!

And if you are struggling with anything, post your issue in the comments and I’ll get back to you as soon as I can.

Have a wonderful Xpedition!

Next lesson HERE

Hierarchical Design

Reminder Tip:

[5] You can work bottom-up or top-down

That’s it for today!

Save and close your project, and let’s continue next time. Let me know if you enjoyed this tutorial in the comments!

And if you are struggling with anything, post your issue in the comments and I’ll get back to you as soon as I can.

Have a wonderful Xpedition!

Next lesson HERE


 [1]I did not see the 0ohm resistors mentioned in this step? Do they need to be copied and pasted from the first sheet as well?

 [2]additionally, you can use project explorer to search for components within the design, using the “Design – Parts” tab. Up to you if its something you find worth including!

 [3]I really like how you circled what the user should be doing, makes the tutorial easier to go through!

 [4]It was actually your suggestion! So thank YOU 🙂

 [5]EDIT

Shrouk El-Attar

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/electronic-systems-design/2026/11/18/aa-battery-replacement-project-tutorial-6-aa-tabs/