Products

AA battery replacement project tutorial #4:  PMIC

Continue 

This entire project is intended to be done within the free trial period.  

[This is Part 4 of the tutorial, for Part 1 click HERE] 

Open Schematic 

Double click your saved schematic to open and continue where we left off from 

New Schematic Sheet 

Let’s create a new schematic sheet. Do you remember how to do so? 

… Yup! You can just look it up as in the image below: 

Pro Tip:  

You can pin the menus you like anywhere,  

you can also set shortcuts for them,  

OR check which shortcuts already exist.  

You can ask the ✨Product Support Copilot✨ how to do any of this. 

Another Pro Tip: 

There are two types of shortcuts: 

  1. Regular Keyboard shortcuts 
  1. Mouse “strokes” , as in just draw any shape with your mouse! 

There are already default ones set for you, but you can set your own or change the default ones too! 

Design Navigator 

Make sure your Design Navigator is open. If it isn’t, you can use the search tool to find it and pin it. 

You can also right click on the sheet in the Navigator to rename it:

PartQuest – Reminder! 

Here is what we covered in the previous lesson about how to import parts.  

Refer to this for the next section! 

Reminder Start: 

Using the Search Tool again, look for PartQuest and click it 

In the search box, look up our battery charger by entering its part number MCP73871-2CCI/ML as in the image below 

Drag and drop the part into your Project Explorer menu as in the image below 

Click and drag into your schematic as in the image below 

Reminder End 😏 

External Components 

Now, let’s use this reminder to find the following components and add them to your schematic: 

  1. ERJ3EKF1001V  
  1. MCT06030C1002FP500  
  1. 150060GS75000  
  1. 150060SS75000  
  1. SMLEN3BC8TT86  
  1. CL21A106KOQNNNE  
  1. B57620C5103J062  
  1. RC0805FR-0710KL  
  1. RC0603FR-07100KL  

Arrange Components 

Arrange your components so that they look something like the image below. 

Circled in yellow are 0R resistors. They appear a different size for now, but we will cover this in the next step! 

Pro Tip:  

Click CNTRL + R to rotate components 

ANOTHER Pro Tip:  

Want to turn off pin number attributes? 

Of course, you can ask the Product Support Copilot how to. But here’s a quick way to do it: 

  1. Double click the actual PIN itself

2. When the properties tab opens, simply untick the pin number

Scale Components Symbols (grow/shrink) 

You might want to make your 0R links smaller than the rest of the components. If so, the steps are: 

  1. Click the component you want to scale to a different size (I did this for all the 0R)

2. In the search tool, look up “scale” 

3. Choose the scale factor you like

Place Power Symbols 

There are many ways to place a power symbol.  

My favourite is always to find anything I want through the search bar as in the following image. 

Once you place it, you can right click to select properties, and change its Global Signal Name property. 

Create three: 

  1. VUSB 
  1. V_BUCK_IN 
  1. VBAT 

Place them as in the following image: 

Place Ground 

You guessed it, you can just look this one up too!

Now place GND as in the following image: 

Place Net 

Pro Tip:  

Click n (lower case) to place a net 

So go do your thing and place nets to connect components as in the following image:

Place Text 

Yup, look it up through the search bar and you can find it in an instant! 

Now, can you guess how to edit it? 

If you guessed right click → properties, then you’re absolutely correct! 

Place text as in the image below, or wherever you see fit:

Import Image 

I like to import relevant equations from the datasheet. You can use screenshot copy/paste to import equations if you like. 

Reference Designators 

We will do this at the very end, so worry about this for now! 

That’s it for today! 

Close your project, and let’s continue next time. Let me know if you enjoyed this tutorial in the comments! 

And if you are struggling with anything, post your issue in the comments and I’ll get back to you as soon as I can. 

Have a wonderful Xpedition! 

Next lesson HERE

Shrouk El-Attar

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/electronic-systems-design/2026/11/06/aa-battery-replacement-project-tutorial-4-pmic/