Products

Seven ways to make your PCB easier to build

Designing a printed circuit board (PCB) takes more than getting the layout right. The choices you make about materials, features and specifications can affect how easily a fabricator can build the board, and how much it costs or how long it takes.  

In a recent episode of The Printed Circuit Podcast, host Steph Chavez invites John Johnson of American Standard Circuits to share a wish list from the factory floor. The message is direct: bring your fabricator into the conversation early. Their experience can help you make informed trade-offs, avoid preventable delays and deliver a board that meets its requirements without unnecessary complexity. 

Wish #1: Call us before you finalize the design 

The earlier you involve your fabricator, the more options you have. They can advise you on material availability, manufacturing processes and design choices while you can still make changes.  

That matters when materials have long lead times: some can take 13 weeks (about 3 months) or more to arrive. Your fabricator may know which alternatives are available and can still meet your electrical, thermal or mechanical requirements, and a brief conversation early in the process can help you avoid discovering a supply problem after you have completed the design. 

Wish #2: Don’t design to the top of our capability list 

A capability list describes what a fabricator can build. It does not mean your design needs the most advanced feature on the list. 

The finest line width or tightest tolerance can increase cost and manufacturing risk without improving the board’s performance, and combining several advanced features can make the build more complex still. Johnson’s advice: start with what your design needs to do, then work with your fabricator to choose the features that meet those needs. 

That approach helps you avoid paying for capability you don’t need, and makes it easier to balance performance, cost and manufacturability.  

Wish #3: respect what solder mask does 

The solder mask does more than give a board its color. It protects copper and defines the areas where components will be soldered. As features get smaller, mask thickness and registration become more important. 

Johnson points to a common design trap: mixing solder-mask-defined pads with copper-defined pads considering how the mask will register to them. That can complicate fine-pitch assembly. A mask that is too thick can also make it harder to apply solder paste in very small pad areas. 

Ask your fabricator to review pad definitions, mask clearances and coating thickness, especially when your design uses ultra-high-density interconnect (UHDI) features. Their input can help you avoid a detail that creates trouble later in production.  

Wish #4: Understand the cost of complexity 

Stacked microvias and sequential laminations can help route dense designs. They also add manufacturing steps. Each additional drilling, filling and lamination cycle takes time and can increase cost. 

Johnson notes that complex designs with multiple subassemblies can face lead times of 20 weeks (about 4 and a half months) or more. Before committing to that structure, ask whether another layer arrangement or via strategy could meet the same requirements with fewer steps. Your fabricator can help compare the trade-offs and identify options that preserve performance while reducing build complexity. 

Wish #5: Send a clean, consistent data package 

Clear design data helps the manufacturing team understand what you want them to build. Label files with the part number and revision. Keep layer names consistent across the data package and fabrication drawing. Check that the notes describe this design, not a previous one.  

ODB++ can help organize design data, and fabricators can work with Gerber files. Whichever format you use, make sure the package tells one clear story. Conflicting layer names or boilerplate notes can prompt questions and put the job on hold. Remove requirements that don’t apply and ask your fabricator for help if you’re unsure how to specify something. 

Wish #6: Tell us why a specification matters 

A specification tells the fabricator what you want. The reason behind it helps them understand what the design needs to achieve.  

Are you aiming for a specific radio frequency (RF) characteristic, managing heat or fitting the board into a tight space? Share that context. Your fabricator may be able to suggest a different tolerance, material or process that meets the same design intent.  

When you explain the “why,” you give the manufacturing team a chance to solve the problem with you, not just flag a requirement that may be difficult to meet.  

Wish #7: Remember that your design joins a queue 

Manufacturing engineering teams review many jobs at once. Johnson describes teams handling 70 to 100 jobs. A straightforward design with clear data may move through review quickly. A job with unclear notes, unavailable materials or unresolved manufacturing questions may wait while the team sorts out the issues. 

You can help your design move forward by preparing a complete package, checking material availability, and resolving manufacturability questions early. That gives the fabricator a clearer path from design review to production. 

One last wish: Keep talking 

The factory floor’s wish list comes down to one practical step: involve your fabricator early and keep the conversation going. Share what the board needs to do, ask for feedback and stay open to options that meet the requirements with less risk. 

As Johnson states, “Call us, email, text me.” The right conversation can help you simplify the design and build a board that meets its requirements without added cost or delay.  

Regan Sumy
Content Marketing Intern

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/electronic-systems-design/2026/11/09/seven-ways-to-make-your-pcb-easier-to-build/