Products

Your #1 defense against a crosstalk crisis

It’s been some time since I’ve seen an article on crosstalk, so I decided to take the opportunity to walk through the subject in a soup-to-nuts overview for those in the PCB design community that may be interested in why crosstalk-savvy PCB designers and hardware engineers use various design rules for controlling crosstalk.  In the process of doing so, we’ll identify which design tweaks provide the most leverage for controlling far-end crosstalk.

Here, we’ll focus on edge coupled signal-to-signal crosstalk.  If you’d like to know more about managing crosstalk in the z-direction, check out my recent webinar, Interplane Crosstalk and Dielectric Selection in PCB Stackup Design.       

Introduction to Digital Crosstalk

Crosstalk is unwanted noise generated between signals. It occurs when two or more nets on a PCB are coupled to each other electromagnetically (even though conductively, they’re not connected at all). Such coupling can arise any time two nets run next to each other for any significant length. When a signal is driven on one of the lines, the electric and magnetic fields it generates cause an unexpected signal to also appear on the nearby line, as shown in FIGURE 1.

PCB crosstalk example
FIGURE 1. Crosstalk occurs when two or more neighboring traces couple together.

A number of factors combine to create an unwanted crosstalk signal: the length over which the traces are coupled, the distance between the traces, their positions in the PCB stackup, what driver ICs are used on both the “aggressor” and the “victim” lines, whether or not the lines are terminated, and so forth. Crosstalk is a particularly hard phenomenon to anticipate and control unless you’re able to simulate it, because there is almost no way of intuitively knowing how much crosstalk voltage and current will develop due to a given coupling.  Nevertheless, there are semi-conservative design guidelines that can be useful—though almost always at the expense of board real estate.

Crosstalk definitions

In crosstalk parlance, the “aggressor” signal or trace switches and causes crosstalk.  The “victim” signal or trace responds by developing an unintended signal.  The effect is 3-dimensional in nature.  Victims can be adjacent on the same layer or above or below the aggressor, as shown in FIGURE 2.

example of vertical crosstalk
FIGURE 2. Victim nets can be above, below, or adjacent to an aggressor net.

Actually, two coupled signals are imposed upon the victim net: a forward signal, and a backwards signal.  The “forward” pulse travels along with the aggressor’s signal; and a “backward” pulse travels back from the aggressor signal.  Crosstalk at the victim’s far end is called “far-end crosstalk,” or FEXT, and coupled voltage at the near end is called “near-end crosstalk” (NEXT).  FIGURE 3 shows both forward and backward crosstalk.

image showing an aggressor trace and victim trace with forward crosstalk pile up and backward crosstalk
FIGURE 3. An illustration of both forward and backwards crosstalk on a victim trace.

The backward signal often ends up traveling forward after reflecting off of a driver. 

Current is injected into the victim by electric fields (the lines that run orthogonal to the traces in FIGURE 2) that are caused by capacitive coupling interactions between the aggressor and victim nets.  These interactions are affected by conductor surface area and distance, and generally terminate at adjacent conductors.

Voltage is induced on the victim by magnetic fields.  These are inductive (transformer) coupling interactions, which are somewhat circular—surrounding the aggressor and victim nets.  These interactions are not generally stopped by conductors, and can therefore extend around multiple adjacent conductors.

Crosstalk guidelines

The most common crosstalk design rules involve trace-to-trace separation.  A PCB designer might, for example, set an auto-router to 4-mil trace width and 4-mil spacing.  This will, of course, maximize router completion, but the resulting design will incur 20-60 mV of crosstalk.  Adjusting noise-sensitive victims to more than 6-mil trace-to-trace spacing can help avoid this problem, as shown in FIGURE 4.

a graph showing the relationship between trace to trace separation and overall crosstalk voltage
FIGURE 4. Using two parallel, 5-inch lines, the graph shows the curves for NEXT and FEXT beginning to flatten out at around 7-mil spacing between aggressor and victim nets. Tighter spacing, to the left of the vertical line, results in more crosstalk, and wider spacing – to the right of the vertical line – results in diminishing benefit.

Dielectric effects and reference-plane distance

Since electric fields terminate at reference planes, traces close to reference planes have reduced crosstalk.  Capacitive trace-to-trace coupling drops off quadratically with the distance from the reference plane(s)—so traces within 4 mils of a reference plane will be much more immune to crosstalk than a trace 6 or more mils from the nearest reference plane.  And symmetric striplines—because of their relative proximity to not one, but two reference planes—have relatively higher immunity than microstrip signals.

Moreover, there’s a dielectric-constant effect to consider.  High dielectric constants (Dk) concentrate the electric field, resulting in relatively poorer crosstalk performance, in a roughly linear relationship between Dk and capacitive crosstalk. 

Example: Crosstalk on a bus

Suppose you’re designing a bus, and you want to guarantee that no more than 200 mV of crosstalk can occur on any of the signals. Let’s go through the process of developing the proper routing constraints to achieve it.

A typical bus in a modern digital system contains many physically parallel traces—16, 32, 64—maybe even more signals. However, to analyze crosstalk on such a bus, you can narrow the scope to a single “victim” trace, with “aggressor” nets on either side.

Let’s start with coupled, coplanar 6.0-mil wide (W) striplines, running parallel for 12 inches with trace-to-trace separation of 8.0 mils (S), through a 4.3 Dk dielectric with a 5.0 mil height (H), as shown in FIGURE 5.

HyperLynx cross talk simulations for signal integrity
FIGURE 5. Crosstalk is easily illustrated with the aggressor-victim-aggressor example shown. (Shown with Mentor’s HyperLynx LineSim.)

A simulation with HyperLynx LineSim, shown in FIGURE 6, shows the far-end crosstalk to see how much crosstalk occurs with the initial arrangement.  

graph showing voltage vs time on a victim net
FIGURE 6. Far end crosstalk (FEXT) on the victim net shown in Figure 5.

With 590-ps (0.59 ns) driver-switching speeds on the two aggressor nets, and no signal injected on the victim net, we can see about 600 mV on the positive side that will be injected into the far-end victim waveform; and 660 mV on the negative side—both well beyond our design criteria of 200 mV maximum crosstalk.

Crosstalk is a complex effect that is influenced by many different geometric factors: e.g., driver-IC technology (Tr, Tf, output impedance, and drive strength), trace width (W), copper weight (T), parallel-line length (Lp), trace separation (S), PCB stackup (layer ordering, Dk, and dielectric thickness (H)), and line-end termination (crosstalk generally requires more-complex termination than single-line reflections).   Rules-of-thumb exist for controlling crosstalk, but if you really want to know how to minimize crosstalk while controlling cost on your specific design, you need a good simulation tool.  In the following section, we’ll go through an iterative process for dealing with crosstalk on the design in FIGURE 5 and FIGURE 6, and see if some reasonable design rules emerge.

Copper thickness

A crosstalk lever that might be overlooked sometimes is the copper thickness.  In the example above, signals have used 1-ounce copper.  That’s pretty thick for a signal trace.  One might think that reducing copper thickness will reduce capacitive coupling, though simulation shows that the result doesn’t turn out to be significant in practice.  Nevertheless, for the remainder of this discussion, we’ll use the more common, half-ounce copper.

Reducing parallel coupling length to decrease crosstalk

One possible technique for reducing crosstalk is to reduce the length over which aggressors and victims run parallel to one another.  This poses some practical problems on the routing side—as those traces ended up being parallel on a board for a reason—but it’s instructive to see what happens when the parallel coupling region is reduced from 12.0 to 6.0 inches.  Surprisingly, this change doesn’t end up reducing crosstalk at all—simply moving peak crosstalk amplitudes to the left in the time domain.  Reducing parallelism alone, as a crosstalk lever, isn’t quite as powerful as we might think it is.

Increase trace separation to decrease crosstalk

Another common way to decrease the crosstalk is to increase the separation, S, between the traces.  Increasing trace separation from 8 to 12 mils results in a reduction of crosstalk to 400 mV on the positive side, and -400 mV on the negative side—still well beyond where we would like to be; and in the process of making this change we’re using up a good bit more board space.

Modifying the dielectric material

There are many ways besides trace separation and length parallelism to affect crosstalk. One that is sometimes overlooked is the PCB stackup. Recall that we started with a Dk=4.3.  What happens if we try to reduce capacitive crosstalk by using a lower-Dk material, say D=3.8?  Through simulation, it turns out that the improvement from this change alone is negligible; however, in the process of using half-ounce copper, and reducing the Dk of the dielectric, trace impedance increased from roughly 50 ohms to just under 57 ohms.  (Remember: Impedance is inversely related to the square root of trace capacitance, which is tied to the Dk of the dielectric.) 

So, reducing the dielectric thickness (H) from 5.0 mils to 4.5 mils between the stripline layer of interest and the nearest reference plane increases the capacitance again, pulling the impedance back to around 50 ohms.  The combination of these factors gets us much closer to our goal, resulting in 211 mV on the positive side down to about 230 mV on the negative side—more than a 60 percent improvement, but still above our target of 200 mV. 

Reducing trace width (W), which increases impedance (Z0), and then narrowing the dielectric thickness (H) to pull the impedance back down to around 50 ohms is another potential way to reduce crosstalk.  Reducing W to 5.0 mils, and H to 3.75 mils results in roughly 200 mV of both positive and negative crosstalk.

By narrowing trace width (W) by 1.0 mil, the overall bus width decreased in mils by the number of bits minus one.  With an interest in gaining more margin—while keeping the overall bus width as in the initial design—adding another mil to the spacing (i.e., taking S from 8.0 to 9.0 mils) results in plenty of margin: 160 mV on the positive side, and 170 mV on the negative side.  The following table summarizes effects on the topology in FIGURE 5, and their relative impact on FEXT—ranked by relative reduction in worst-case crosstalk.

RankDescription% FEXT Reduction
Original configuration: W=6 mils; T=1oz; Lp=12 mils; S=8 mils; Dk=4.3; H=5 mils0%
Reduce copper thickness (T) to 1/2 oz~0%
Reduce parallel length (Lp) from 12 to 6 mils~0%
4 Increase trace separation (S) frm 8 to 12 mils33%
Reduce capacitive crosstalk: Dk=3.8~0%
3T=1/2 oz; Dk=3.8; H=4.560%
2Reduce W from 6.0 to 5.0 mils and increase H to 3.75 mils65%
1Reduce W from 6.0 to 5.0 mils, H to 3.75 mils, and increase S to 9.0 mils75%
TABLE 1.  Simulation results for reducing the crosstalk shown in FIGURE 5 and FIGURE 6.

FIGURE 7 shows the top four ways of reducing crosstalk on this particular bus design.  The resulting design rule is to use W=5.0 mils, Dk=3.8, H=3.75 mils, and S=9.0 mils.

reducing crosstalk illustrated
FIGURE 7. Top four ways of reducing crosstalk on FIGURE 5 bus design. Resulting design rule is W=5.0 mils, Dk=3.8, H=3.75 mils, and S=9.0 mils.

Parting thoughts

As I’ve been trotting around talking to engineers and PCB designers for the last 10-15 years, I’ve heard many references to the use of thinner dielectrics, so for some readers the contents of this article may be review.  But I haven’t yet seen an article that compared the different levers for controlling crosstalk, with emphasis on the fact that material selection and specifically laminate thickness plays the most pivotal role in controlling far-end crosstalk (FEXT).

If you’d like to know more about controlling crosstalk, check out my recent webinar, Interplane Crosstalk and Dielectric Selection in PCB Stackup Design, where I cover methods for controlling z-direction crosstalk up and down the stackup, including microstrips, signal-signal crosstalk for dual striplines, power-signal crosstalk, power-power crosstalk, and pairing power-ground planes for PDN design.       

Bill Hargin
Chief Everything Officer
This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/electronic-systems-design/2025/07/10/crosstalk/