Products

The virtuous cycle of silicon: How Siemens is accelerating the era of Physical AI with NVIDIA cuLitho

GPU-accelerated computational lithography with Siemens Calibre and NVIDIA cuLitho

By Dr. Jim Shiely, Chief of Staff for Calibre Semiconductor R&D, Siemens EDA 

Siemens and NVIDIA are accelerating computational lithography by integrating NVIDIA cuLitho with Siemens Calibre®, delivering up to 12x speedup across selected lithography workloads.

When people talk about “Physical AI,” they usually imagine autonomous vehicles navigating city streets or humanoid robots working on a factory floor.

But long before today’s AI wave, computational lithography was already operating according to many of the same principles. It observes the physical world, builds models of it, optimizes decisions, acts through physical machinery, measures the result, and uses that evidence to improve the next cycle.

For decades, computational lithography has operated within semiconductor fabs and photomask shops as an ultra-precise closed-loop intelligence system. Software predictions become mask geometries. Those geometries shape the behavior of light. Light exposes patterns in resist. Those patterns are transferred into physical structures on the wafer. Measurements of the resulting silicon structures then provide evidence for the next generation of models and corrections.

Without this intelligent loop, it would not be practical to make the enormous number of coordinated, highly precise decisions required to manufacture the world’s most advanced integrated circuits.

In our official October 14, 2026 announcement, Siemens Digital Industries Software and NVIDIA unveiled a significant advance in this journey. By integrating NVIDIA cuLitho, a CUDA-X library for GPU-accelerated computational lithography, with Siemens Calibre, we are delivering up to 12x acceleration for lithography optimization workloads such as optical proximity correction (OPC).

This collaboration does more than speed up runtimes. It dismantles one of the central computational bottlenecks facing the manufacture of the next generation of AI compute and memory devices: optimizing increasingly complex photomask patterns at leading-edge process nodes.

This milestone advances that cycle through NVIDIA accelerated computing, bringing GPU acceleration to Calibre’s physics-based simulation and optimization workflows.

Why High-NA EUV increases computational lithography workloads

As our industry advances toward angstrom-era nodes and transitions to High Numerical Aperture Extreme Ultraviolet (High-NA EUV) lithography, the lithography problem becomes remarkably difficult.

Shrinking dimensions, complex optical interactions, three-dimensional mask effects, resist behaviors, manufacturing variation and tighter pitch limits must all be accounted for with extraordinary mathematical precision. 

The shapes drawn by chip designers cannot be directly transferred to the photomask and expected to print accurately on the wafer. Diffraction and other physical effects distort the image.

Optical proximity correction (OPC) compensates for these effects by deliberately modifying the edge placements of design patterns written onto the photomask. Inverse lithography technology (ILT) goes further. Instead of beginning with a conventional mask shape and making a series of localized edge corrections, ILT gives the optimizer far more freedom to determine the mask geometry needed to produce the desired wafer pattern.  The solution can yield complex, curvilinear mask shapes. Applied appropriately, those shapes improve pattern fidelity, reduce placement error, eliminate lithographic hotspots and improve yield.

But additional freedom comes at a computational cost.

Full-chip curvilinear ILT and OPC require repeated iterative simulations to optimize pattern shapes across enormous layouts. Computational lithography combines electromagnetic and optical modeling, photochemistry, computational geometry, iterative optimization, and distributed computation. It has been described as the largest compute workload in the semiconductor production process.

Without acceleration, engineering teams face agonizing trade-offs:

  • Restrict advanced ILT to small critical hotspot areas rather than applying it full-chip, foregoing possible improvements in yield.
  • Dedicate massive CPU-based computing infrastructures running for weeks, straining project schedules and power budgets.
  • Compromise project schedules and time-to-market.

To meet the growing demand for the multi-billion-transistor chips powering the AI revolution, these trade-offs are difficult to sustain.

How Siemens Calibre and NVIDIA cuLitho accelerate computational lithography

To solve a compute problem of this magnitude, you need accelerated computing built specifically for the structure of the workload.

NVIDIA cuLitho provides optimized tools and algorithms for accelerating computational lithography on GPUs. By integrating cuLitho with Siemens Calibre manufacturing software, we have transformed a computational bottleneck into a high-throughput manufacturing computation engine.

As detailed in October 14, 2026 announcement , verified engineering data demonstrates:

  • Up to 12x  speedup across key computational lithography and simulation workloads.
  • Simulation speedups ranging from at least 10x to 17x across selected lithography workloads.
  • The computational headroom needed to make practical full-chip optimization using advanced curvilinear methods such as ILT.
  • The potential for energy and datacenter footprint reduction, by accelerating computational lithography workloads on NVIDIA GPUs.

For photomask makers and chip builders, turnaround times shrink from weeks to days. And when simulations run faster, teams can also explore more alternatives. They can apply sophisticated optimization to larger portions of a design. They can investigate difficult patterns sooner. They can perform more iterations before committing a design to mask manufacturing. And they can meet their demanding delivery schedules.

The virtuous cycle of compute

There is a poetic symmetry at work here: GPUs are now accelerating the design and manufacturing of the next generation of GPUs.

The cycle works like this:

  1. NVIDIA Accelerated Computing: NVIDIA GPUs execute cuLitho-accelerated Calibre workflows.
  2. Computational Lithography: Physics-based simulation and optimization determine the photomask geometries needed to print increasingly difficult patterns.
  3. Advanced Silicon: These photomasks enable manufacturers to achieve the pattern fidelity and process margins required for leading-edge silicon.
  4. Next-Generation AI: The resulting silicon powers the next generation of AI and accelerated-computing clusters, which in turn accelerates future chip design and manufacturing.

Hardware accelerates the software. The software helps create better hardware. That better hardware returns to accelerate the next cycle.

This self-reinforcing loop will become an important mechanism for sustaining continued semiconductor scaling and performance improvement in the decade ahead.

Grounded in physics, accountable to silicon

In an era crowded with claims about generative and agentic AI, it’s worth emphasizing what makes this milestone distinctive: physical accountability.

In computational lithography, software output is immediately tested against relentless physical laws. If a simulated contour doesn’t match the etched silicon wafer, yields collapse. Trust isn’t built on software claims; it is earned on the wafer.

By combining the established role of Siemens Calibre in semiconductor verification and manufacturing with NVIDIA’s accelerated computing architecture, we are giving the semiconductor industry a scalable, production-ready foundation.

The road to angstrom-era computing requires mastering the physics of the unimaginably small. Together with NVIDIA, Siemens Calibre® is making sure compute power is no longer the obstacle standing in the way.

Read the Announcement & Learn More

Calibre IC Design & Manufacturing

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/calibre/2026/10/14/the-virtuous-cycle-of-silicon-how-siemens-is-accelerating-the-era-of-physical-ai-with-nvidia-culitho/