Products

New in Solid Edge 2025: Sheet Metal

Take a deep dive into everything new in Solid Edge 2025 with a series of blog posts focused on the exciting new features and enhancements in this year’s release. In this blog, learn more about the exciting sheet metal enhancements in Solid Edge 2025. 

Elevate sheet metal design with new etch and bend features 

Continual improvements to Solid Edge’s industry leading sheet metal capabilities streamline workflows and improve precision. Etch features are now supported across bends and curved faces. The etch is automatically placed on all faces touched by the wrapped input geometry, and the command automatically remembers the last options you used for easier replication in the future. The etch geometry also adjusts correctly on bend regions when the sheet metal flat pattern is created.  

The improved curve connectivity across face edges with the Wrap Sketch command guarantees curves lay on parent surfaces and improves the wrapping around closed loop faces. These improvements are implemented in both the assembly and part modeling environment, increasing the reliability and accuracy of your wrap sketch results. 

New bend deduction and bend allowance in bend length calculations for sheet metal allow you to control material conditions related to manufacturing and tooling. You can select the bend calculation method, edit in the spreadsheet and customize the specific settings for bend equations. This ensures your designs translate seamlessly from the digital twin to the physical part, minimizing errors. 

The Inquire Elements command supports the new bend calculation methods, showing bend properties, calculation method, Microsoft Excel® file information and neutral factor in use by the specified individual feature. You are now able to know exactly which properties and neutral factor are used on a specific bend whether editing the default value or retrieving it from the Excel gage table. 


Join the conversation   

All of these new features and enhancements in Solid Edge 2025, along with many more, were announced during our live premiere on October 23, 2024.   

To learn more about what’s new in the Solid Edge 2025 release, click here.  

There are a lot of ways to hear what others are saying about the upcoming release and to connect with other Solid Edge enthusiasts online.   

Here are a few ways to join the conversation right now:   

  • Join our vibrant online Solid Edge Community to connect and interact with other Solid Edge users.   
Kyzmen Wood

Comments

One thought about “New in Solid Edge 2025: Sheet Metal
  • When will you make the Sketch better => now it is very difficult to find the error in the sketch if you change a higher item.
    The rest is OK but the sketch is the worst I have ever worked with.

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/solidedge/solid-edge-2025-sheet-metal/