Products

What is Simulation-Driven Design for Manufacturing?

As simulation technology has become more and more adept at modeling real-world product behavior, companies have increasingly embraced the benefits of simulation-driven design for manufacturing, optimization, and virtual testing. In an effort to increase innovation, cut
costs, and streamline design and production schedules, implementation of simulation-driven design practices throughout the product development cycle have proven to be key to staying ahead of the competition. 

An often overlooked aspect of product design and simulation, however, is part manufacturability. A simulation-driven design on a computer screen might not exactly match what ends up being manufactured, or even be possible if part details cannot be executed by the chosen
manufacturing method. Discrepancies between virtual and physical prototypes can end up being a major burden at such a late stage in the product development process. For example, on average, correcting defects during a mold trial adds an additional
26% to the total cost of the mold, according to a survey conducted by Tech-Clarity. The choice
of manufacturing process, materials used, and machine tolerances can dramatically affect what designs can be efficiently produced and how well that part performs compared to its virtual counterpart. 

Trial-and-error approaches can make it difficult to anticipate manufacturing issues and know how best to correct them. This often results in engineering teams committing time and resources to modify designs and physically retest new prototypes, and as
a result, parts run the risk of being over-engineered, adding cost and negatively impacting performance.  

By contrast, a simulation-driven design for manufacturing (SDfM) approach delivers manufacturability insights directly into the hands of product designers. Design flaws can be detected and corrected early, allowing users to confidently design
to their chosen manufacturing method. Designing for production right the first time helps bring products to the market faster and enables the exploration of more cost-effective workflows for additive manufacturing, casting, molding, metal forming,
and more.

 

Addressing Design for Manufacturing Challenges with Simulation-Driven Design

When designing products, manufacturers typically run into challenges involved with cost, development and production speed, and maintaining quality at scale. Rather than moving back and forth between CAD tools and simulation models, users want to perform
quick evaluations without needing to be a CAE expert. 

Altair Inspire™ is well-suited for upfront simulation-driven design, allowing teams to collaborate, quickly evaluate and modify designs,
and rapidly converge on an optimal path forward. 

A collage of four images: A cycle featuring industrial design; a close-up of an element showcasing computational physics; a simulation-driven design of a machine part; and A process defining manufacturability.

Each of the four categories above – design, physics, ideation and optimization, and manufacturability – play a major role in the success of a simulation-driven design. The Inspire family of products provides users all of these tools together in one unified user
interface.

 

Solver Power for Every Step

Inspire users never have to compromise accuracy for speed because dependable Altair solvers power all tools within the platform. For example, structural analysis can be run with Altair SimSolid™, which is integrated into Inspire. The same goes for multibody dynamics analysis and topology optimization. Altair’s dynamic motion simulation and structural analysis solvers are also integrated
with Inspire, making geometry creation, structural optimization, and assessment of mechanisms a seamless process.

 

Integrating Simulation-Driven Design with Manufacturing

Altair offers a unique set of simulation tools for manufacturers of all experience levels to evaluate product feasibility, optimize the manufacturing process through SDfM, and run virtual try-outs for many traditional, subtractive, and additive manufacturing
processes. Users can validate designs early in the manufacturing process with the simplicity and affordability of the simulation-driven design software, as well as use optimization technology with specific manufacturing constraints to design better, more efficient
products.

A visual representation of the steps in simulation-driven design

Generate designs, simulate, and analyze results with Altair Inspire

Additive Manufacturing

Let’s take 3D printing, for example. Altair additive manufacturing (AM) software goes beyond the creation of unique prototypes and provides a robust simulation toolchain to support production designs. Altair Inspire Print3D can cut product development and AM costs by reducing material usage, print times, and post processing. It also provides a fast and accurate toolset
for the design and process simulation of selective laser melting (SLM) parts. 

Design of a large engine pylon structure
By utilizing Altair HyperWorks™, SOGECLAIR Aerospace streamlined
the design of a large engine pylon structure using topology optimization to reduce weight on the component. 
 

Molding

Advanced injection molding can easily be performed through a five-step workflow with Altair Inspire Mold. Virtual testing, validation,
correction, and optimization of molding designs are all features within the software, which provide insights to evaluate injection molded part manufacturability. Common manufacturing defects such as warping, sink marks, and short shots can be corrected
early by product designers and engineers, long before a mold is made. 

Injection molding overview

“We use OptiStruct, an Altair software solution, for topology optimization. With this solution we were able to build injection molds which weigh only 25 percent of the original part. This means we saved 75 percent of weight on each tool.” – Ralf Gärtner, unit leader at Phoenix Contact and managing director at Protiq GmbH.

Metal Forming

Altair Inspire Form offers a fully integrated solution for enhanced sheet metal forming, product feasibility, detailed process analysis
and virtual try-out. As a complete stamping simulation environment, product and process engineers can utilize the software’s highly scalable incremental solver to accurately analyze material flow, splits, wrinkles, loose metal, and springback.
The solver supports multistage forming and trimming and enables the production of high-quality parts in a modern and intuitive user interface. 

Altair Inspire Form virtual stamping tryout

Casting

Fast, accurate, and affordable, Altair Inspire Cast is the only tool that caters to beginners and experts alike, from product
designers to foundry engineers. Guided process templates offer five easy steps to simulate gravity die, gravity sand, investment, high pressure, low pressure die casting, and tilt pouring.

Altair Inspire Cast overview

“We have seen significant time and cost savings while using Altair Inspire Cast: €5,000-10,000 and 3 weeks for actual trials vs. €500-600 and 1 day of simulations in Altair Inspire Cast.” – Ahmed EL ABIDI, CAE manager and senior expert, U-Shin

Extrusion

Altair Inspire Extrude is an easy-to-use platform for both metal and polymer extrusion simulation. Using Inspire Extrude Metal, CAD can be quickly de-featured and modified inside the tool, ensuring potential profile distortion, damage from deflection,
backend contamination, charge weld defects, bad seam weld, bad grain size, overheating profile quality, and poor surface quality issues are corrected early in development. With Inspire Extrude Polymer, users can increase their understanding of how
profile features and process variables interact for any particular metal alloy. Learn more about
how the Extrude Metal workflow can be implemented, demonstrated by a typical workflow for metal extrusion simulation.  

Altair Inspire Extrude Polymer overview

Polyurethane Foaming

With Altair Inspire PolyFoam, manufacturers can efficiently simulate polyurethane molding and foaming processes early to improve
product quality and cycle time and reduce scrap and tooling rework costs. The software has the ability to inject multiple foams into the same mold simultaneously and allows for quick and accurate simulation of different foam compositions. An
easy-to-use, five-step workflow with
Inspire PolyFoam ensures that foam product designs can be validated fast and efficiently.   

Altair Inspire PolyFoam overview

Altair Simulation-Driven Design for Manufacturing

When developing a new product, manufacturers want to be sure their development process is going to be as efficient as possible. With a SDfM approach, product designers can be confident in their chosen manufacturing method because design flaws
can be detected much earlier and corrected before any physical prototyping has to be done. Implementing simulation-driven design early allows engineers to create innovative, manufacturable products beginning at the earliest stage of production. Altair Inspire™
products cover all facets of manufacturing, from casting and PU foaming, to extrusion and metal forming, allowing for quick, generative design for manufacturing processes.

Click here to learn more about Altair’s simulation-driven design for manufacturing solutions.

Daniel Santoro

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/what-is-simulation-driven-design-for-manufacturing/