Products

Kettering University reduces undesired EV motor noise

Electric vehicle (EV) motor noise can be annoying. How can you reduce it? Addressing the challenges of electrification, the students of the Kettering University deployed methods to help reduce undesired EV motor noise.


In today’s automotive industry, it becomes clear that electric vehicles (EVs) are the future of mobility. Internal combustion is less attractive. As a result, manufacturers are looking for better ways to develop and design electric engines. One might assume that those people conducting research on EVs are looking for ways to enhance long-distance performance. However, in this instance, the issue is less about optimizing travel and more about enhancing comfort. Indeed, in electric vehicles, the high-frequency noises from tires or electrical accessories become more prominent. As a result, Kettering Universities engineering students have been studying the causes of high-frequency vibrations within e-motors.

Three-stage analysis

The study entails three parts: electromagnetic analysis, structural analysis, and acoustic analysis. Kettering’s goal was to develop a cost-effective method for reducing noise caused by these vibrations. The engineers began by analyzing the sound generated by an electromagnetic model of a three-phase induction motor via simulation. To validate these simulation results, the engineers had to conduct an acoustic test on a small-scale general-purpose motor. 

A student performs EV motor noise measurement in an anechoic chamber
Measuring EV motor noise in an anechoic chamber

Kettering’s engineers utilized Simcenter Testlab during both the structural and acoustic analysis on the motor. The acoustic analysis assisted engineers in identifying frequencies at which sound pressure peaked and offered insight as to how to isolate those. The test also involved the creation of a spherical mesh with microphones around the motor. These microphones were placed approximately one meter from the motor (as seen in pink below). 

Field point mesh image
Field point mesh

Eventually, an operational modal analysis visualized specific motor vibrations at certain points within the motor. It was then found that frequencies were generating vibrations from within the motor’s housing and its end brackets. As a result, the engineers found that by using modified end brackets, they could simplify the process of isolating frequencies that amplify perceived sound. 

Operating deflection shapes of the EV motor's end brackets
Operating deflection shapes of the EV motor’s end brackets

If successful, Kettering’s study could provide electric motor manufacturers’ a new way of reducing undesired motor noise without adding additional weight. 

Stephen Cortelli

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/simcenter/kettering-university-utilizes-siemens-plm-software-for-game-changing-study/