Simcenter E-Machine Design 2512: Release highlights 

Simcenter E-Machine Design 2512: Release highlights 

The latest release of Simcenter E-Machine Design 2512 brings a suite of powerful enhancements designed to tackle real-world engineering challenges in electric machine design and simulation. Here’s what’s new and why it matters for your workflow.  1. Accurate hairpin winding losses  Why it matters: As electric machines evolve, hairpin windings—especially those with larger solid conductors—face significant AC losses at higher frequencies. These losses, driven by skin...
Advancing Induction Machine and Transformer Workflows – What’s new in Simcenter 3D Low Freq EM 2512 

Advancing Induction Machine and Transformer Workflows – What’s new in Simcenter 3D Low Freq EM 2512 

Faster set-up for an induction machine Induction machines (IM) are the workhorse of industry. Known for their ruggedness, cost-effectiveness, and ability to achieve very high speeds, they...
Rapid axial-flux motor analysis – New in Simcenter E-Machine Design 2412

Rapid axial-flux motor analysis – New in Simcenter E-Machine Design 2412

To build a truly silent machine ultra-precision is required, and any torque ripple needs to be eradicated. One such machine that thrives when given such demands is the air core axial-flux machine. learn more in this blog
Electrification in the USA – Will Palo Alto run out of energy this summer?  

Electrification in the USA – Will Palo Alto run out of energy this summer?  

Simcenter transformer simulation solution is helping transformer OEMs design next-gen grid transformers for the electrification of cities such as Palo Alto. It covers initial sizing for efficiency, solid-insulation assessment, thermal performance, and detailed electrical and mechanical design, balancing multi-attribute performance in terms of efficiency, thermal, structural integrity, and noise. Learn more in this blog
Electromagnetic simulations as part of your design process, that’s EMAG-nificent

Electromagnetic simulations as part of your design process, that’s EMAG-nificent

Electromagnetics (EMAG) and electrical engineers are at home with streamlined EMAG Computer Aided Engineering (CAE) packages, like Simcenter SPEED, Simcenter...
How fast can you simulate a 45 MVA Power Transformer from production CAD import?

How fast can you simulate a 45 MVA Power Transformer from production CAD import?

Simcenter 3D enables you to overcome CAD import bottlenecks in prepping an associative EMAG geometry. When combined with design rules through user-defined parameters, it is possible to automate a power transformer loss analysis workflow, that is responsive to design CAD changes.
Why are power transformers so noisy?

Why are power transformers so noisy?

Reduce power transformer noise in the design stage, with a multi-physics simulation and design approach.
Power busbar design, relax, don’t blow your fuse.

Power busbar design, relax, don’t blow your fuse.

Introduction: DC Circuits Vs The Circulatory System. To better understand a power busbar, we can consider the human circulatory system...
How does cold crucible induction melting ensure titanium purity?

How does cold crucible induction melting ensure titanium purity?

Melting a metal without it touching the crucible walls, is like melting butter without it touching the bowl!
Electromagnetics in the Age of Industry 4.0

Electromagnetics in the Age of Industry 4.0

Imagine our lives without our smart gadgets? La vie without electromagnetics? In fact, go a step further, the very existence of life on earth depends on the Earth’s magnetic field. Without it, solar ...
Introducing Simcenter 3D Low Frequency Electromagnetics 2019.2

Introducing Simcenter 3D Low Frequency Electromagnetics 2019.2

Simcenter 3D Low Frequency Electromagnetics (Low Frequency EM) is part of Simcenter 3D Electromagnetics, which also includes high frequency Electromagnetics. Simcenter 3D Low Frequency EM offers in...
Keeping Traction Motors as “Cool as a Cucumber”

Keeping Traction Motors as “Cool as a Cucumber”

How are cucumber slices placed on the eyes during makeup analogous to motor cooling? The makeup reaction that raises the eyes’ temperature can be seen as the motor loading to meet a certain torque de...
Simcenter Motorsolve Now Exports to Simcenter Amesim

Simcenter Motorsolve Now Exports to Simcenter Amesim

As systems become more electrified, designers are required to ensure compliance of electric drive systems in terms of electromagnetic, thermal, noise, vibration, and structural analysis. Simcenter in...