Corporate

ChatGPT Work mode for sales: Chat vs Work and GPT-5.6 explained

Most salespeople already use ChatGPT. They ask it to improve an email, prepare discovery questions, research an industry or challenge the positioning of an opportunity.

That is useful, but it is still largely conversational. The seller asks a question, receives an answer and decides what to do next.

The introduction of Work mode changes that relationship. ChatGPT can now move beyond helping someone think about a task and begin carrying that task through to a reviewable outcome.

For sales, this is more important than another model upgrade. It represents a shift from AI as an assistant to AI as a delegated member of the workflow.

The mistake will be treating Chat and Work as competing options. They serve different purposes.

Chat is where sellers think with AI. Work is where they delegate structured work to AI.

What Chat and Work actually are

Chat mode is designed for questions, discussion and rapid iteration. It is best when the seller wants to remain closely involved in shaping the answer.

A seller might use Chat to:

  • Test an account hypothesis
  • Practise handling an objection
  • Improve a prospecting message
  • Translate technical capability into business value
  • Think through the next step in an opportunity

The conversation itself is part of the value. The seller is not simply requesting an output. They are using AI as a thinking partner.

Work mode is designed for tasks with a defined outcome. It can work across files, sources, plugins and approved tools, complete multiple steps and produce something that is ready for the seller to review.

That could include creating an account plan from several documents, analysing pipeline data, building a meeting briefing, preparing a presentation or producing a recurring update.

The seller still owns the judgement. The difference is that they are delegating more of the preparation and production.

Why this matters for sellers

Sales teams do not generally suffer from a shortage of information. They suffer from fragmented information and limited time to turn it into action.

Customer notes sit in one place. Opportunity data sits somewhere else. Industry research, enablement content, stakeholder information and previous correspondence all add further context.

Chat can help a seller interpret one part of that picture. Work can bring the pieces together and create a usable result.

This changes where AI can add value. It is no longer limited to making individual activities slightly faster. It can potentially compress an entire workflow, such as moving from scattered account information to a structured meeting strategy.

For sales leaders, the opportunity is not simply higher AI adoption. It is greater consistency in how teams prepare, analyse opportunities and execute repeatable sales motions.

Where GPT-5.6, Sol, Terra and Luna fit

GPT-5.6 should be understood as a model family rather than one universal setting. The best choice depends on the complexity, value and repeatability of the sales task.

Sol is for complex, open-ended work.

This is the strongest fit for high-value activities requiring judgement, deeper analysis and polished outputs. Examples include creating an executive account strategy, analysing a complex competitive position or developing a customer-specific value narrative.

Sol should not automatically be used for everything. Its value is highest when the quality of the result justifies additional processing and review time.

Terra is the everyday workhorse.

Terra is suited to routine sales work that still requires reasoning and tool use. It could support meeting preparation, opportunity summaries, follow-up planning or the creation of first drafts from multiple sources.

For many sellers, Terra is likely to provide the most practical balance between speed and depth.

Luna is for clear, repeatable tasks.

Luna is positioned for specific, high-volume work where the required result is already well defined. Examples include classifying leads, extracting actions from meeting notes, standardising CRM summaries or converting information into a consistent format.

The clearer the task and output standard, the stronger the case for Luna.

The important principle is simple: do not choose the most powerful model by default. Match the model to the commercial value and complexity of the work.

Practical ways sales teams can use both

The strongest workflows will combine Chat and Work rather than force sellers to choose between them.

A seller could use Chat to challenge their assumptions about an account, clarify the commercial problem and define what a good customer meeting should achieve.

Once the direction is clear, they could move to Work and ask ChatGPT to analyse the available material, create the briefing and produce the supporting presentation.

After the meeting, Work could structure the notes and proposed actions. Chat could then help the seller think through stakeholder reactions or refine the follow-up message.

Chat supports judgement. Work supports execution.

A simple way to get started

Choose one sales activity that currently requires several sources or more than 30 minutes of preparation.

Define:

  • The outcome you need
  • The sources ChatGPT should use
  • The audience for the output
  • The format required
  • The points where human review is necessary

Use Chat first if the objective is still unclear. Move to Work once you can describe the required result and what good looks like.

Sales leaders should test this with a small number of repeatable workflows before scaling it across the team. Measure preparation time, output quality, seller adoption and whether the work improves the next customer action.

The wider shift is not from people to AI. It is from prompting for isolated answers to designing better human and AI workflows.

The sales teams that benefit most will not be those using AI most frequently. They will be those that know when to think with it, when to delegate to it and where human judgement must remain in control.

Test Chat and Work on one live sales workflow this week.

About the author

Benedict Russell is a Global Partner Development Executive responsible for scaling global GTM programs across all motions. He helps shape Siemens’ digital selling and AI strategy, embedding best practices that accelerate SaaS adoption and recurring revenue. Previously, he drove partner coverage and expansion, adding 300+ partners to the Siemens ecosystem. Read Benedict’s most recent blog here.

Benedict Russell

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/partners/chatgpt-chat-work-mode-workflow/